PI 073-16 Lohr am Main, 2016-10-19

Powerful performance

With extreme power density and high flexibility, the Hägglunds CAb motors will make hydraulikc direct drives the optimal choice in many applications.

The Hägglunds CAb motor was introduced to the market in 2015 and offers an extreme power density and high flexibility that makes it the perfect choice for applications in need for a small but truly powerful motor.

The motor offers a unique ability to deliver full torque and speed simultaneously bringing customers the power they need when they need it. The unmatched power-to-weight-ratio means energy and production efficiency. Compared to conventional solutions, the CAb motor, provides 10 to 15 percent more torque for the amount of energy put in. Because they weigh so much less, they use less energy in the high-speed range.

Fourteen configurations in small torque steps allow tight dimensioning and optimization in relation to the hydraulic pumps. With only two mechanical interfaces in all configurations, easy adaption is also possible.

The CAb comes with all the benefits offered by the compact Hägglunds motors. These include a built-in ability to withstand shock loads, as well as perfect internal symmetry. The latter ensures consistent torque throughout the revolution, as well as a perfect balance of forces that minimizes noise and vibration.

As of 2016 the Hägglunds CAb is even more suited for many applications with new hydraulic connections and accessories such as through-hole kit, speed sensors and option for vertical mounting.

From unique power density to high energy efficiency, the Hägglunds CAb motor means powerful benefits in industry and beyond.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 31.100 associates generated sales revenue of approximately 5.4 billion euros in 2015.

To learn more, please visit

The Bosch Group is a leading global supplier of technology and services. It employs roughly 375,000 associates worldwide (as of December 31, 2015). The company generated sales of 70.6 billion euros in 2015. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing and sales network covers some 150 countries. The basis for the company’s future growth is its innovative strength. Bosch employs 55,800 associates in research and development at 118 locations across the globe. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.”

Additional information is available online at , ,


Search press releases


Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573

Related Articles

Press Information

Largest flow on the market

Rexroth is raising the bar in performance and communication for hydraulic actuators with its new generation of WRC-4X directional cartridge valves. The valves are more dynamic and consistently achieve flows that could previously only be achieved with the next highest available size. Integrated electronics (OBE) allow the new valve series to be networked via open interfaces with higher-level control units and Industry 4.0 environments even when under analog control. This means that valves can already be integrated into forward-looking automation concepts today.

Press Information

Rexroth offers digitalization of analog interfaces in hydraulics via IO-Link

Reduced connection costs at increased availability: Rexroth harnesses the advantages of the IO-Link open standard also for hydraulic actuators and sensors. As of now, 4WRPEH proportional control valves and HEDE10 pressure switches are available with IO-Link interfaces. Connection is realized via the decentralized and quick IP67 I/O system S67E IO-Link Master. This offers users direct access to the field bus and all data provided by the actuator/sensor.