Press

Content
PI 080-16 Lohr am Main, 2016-11-14

IndraDyn S – MS2N synchronous servo motors extended by additional variants

IndraDyn S – MS2N synchronous servo motors

Modern functionality and customized configurability – the MS2N series is the perfect basis for new machine concepts

Complete, customized and ready-to-use solution for most demanding drive tasks

  • Motor options with forced ventilation and water cooling
  • Increased continuous torques and highest power density
  • New encoder option with certified safety

Modern machine concepts require high-performance drive systems which are flexibly configurable. Consequently, Rexroth has extended their extensive range of the newly designed IndraDyn S synchronous servo motors of the MS2N series with maximum torque from 4 Nm to 360 Nm by force-ventilated and water-cooled variants.

The range of product line MS2N comprises numerous equipment variants. Innovative solutions such as the flexible single-cable and dual-cable connections with quick-look are amended by practical options for holding brake, degrees of protection and encoders in different performance classes, all available in single- and multi-turn. The digital encoder systems with ACURO®link interface allow for the single-cable connection with up to 75 m cable length and offer certified safety according to SIL2 PLd.

This extensive motor kit is now extended by additional functional options. From frame size MS2N07, the motors are optionally available with forced ventilation or water cooling and thus cover the range from 17.5 Nm to 214 Nm continuous torque at standstill with considerably increased power density and highest energy efficiency. Thanks to the additional cooling, new working points with higher continuous torque and higher motor power are achieved without having to change to larger or longer motors. With MS2N10, the fan is completely integrated into the motor and offers this performance advantage in the smallest installation space.

All fan motors offer degree of protection IP65, an integrated temperature sensor with certified intrinsic safety as well as optionally 115 V or 230 V connection voltage.

The cooling circuits of the water-cooled motors are completely designed in stainless steel and allow for the simple and reliable connection to most different machine cooling systems. Water-cooled motors keep the loss power away from the machine. This thermal decoupling allows for the realization of applications with highest requirements on the machining precision.

Two selectable flange accuracies, the sealing air option integrated ex factory and the “Standard” encoder class with Hiperface® interface offer additional configuration options. Despite cost-effective technology, the new encoder option with certified safety according to SIL2 PLd offers the full scope of functions of modern drive technology with motor data memory and real time processing of real motor measurements. The individual measurements of every single motor as well as the saturation and temperature data are stored in the memory of the relevant motor encoder and automatically processed by IndraDrive controllers. This information considerably increases the torque accuracy and reduces the tolerance interval in the ongoing operation to a fraction of present values. It is now possible for the first time to use the servo motor as reliable sensor and as data source and to thus realize new applications in the environment of Industry 4.0, such as condition monitoring, in a cost-effective manner, without additional components.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 31.100 associates generated sales revenue of approximately 5.4 billion euros in 2015.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 375,000 associates worldwide (as of December 31, 2015). The company generated sales of 70.6 billion euros in 2015. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing and sales network covers some 150 countries. The basis for the company’s future growth is its innovative strength. Bosch employs 55,800 associates in research and development at 118 locations across the globe. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.”

Additional information is available online at www.bosch.com , www.bosch-press.com , twitter.com/BoschPresse

 

Search press releases


Contact

Johanna Rauch
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1358
johanna.rauch@boschrexroth.de




Related Articles

2018-06-11
Press Information

Software of the future: Freed from …

…the restraints of hardware – the software of the future. In the factory of the future, machine modules and processing stations will be regularly reorganized, flexibly take on new tasks and retrieve the appropriate software function. This change has already begun: Machine manufacturers are already able to install identical control functions on various device platforms without any extra effort. Here is an overview of concepts for today and tomorrow:


2018-04-11
Statement

The factory of the future – how far we have come and where we are going

Imagine a factory where you could change everything apart from the floor, roof and walls within a few days or even hours? Full flexibility, individuality and scalability. This is exactly what the factory of the future is about.