International
 

Press

Content
PI 077-16 Lohr am Main, 2016-11-21

Industry 4.0 for new and existing machines

Industry 4.0 for new and existing machines

Secure solution for valuable information: The IoT Gateway connects new and existing machines with the Internet of Things (IoT) without intervening in the automation logic.

The IoT Gateway from Bosch Rexroth cost-efficiently makes new and existing plants ready for the Internet of Things

  • Simple connection of machines to IoT software solutions
  • Quick web-based configuration in three steps for a multitude of applications
  • Flexibly integratable system platform based on open software standards

Network existing machines and plants cost-efficiently and improve your production processes or product quality using newly gained information. With the IoT Gateway from Rexroth, connecting to Industry 4.0 environments is possible without intervening in the automation logic. It collects sensor and process data and transfers it to higher-level IT-based solutions such as MES, cloud applications, systems for local monitoring of machine states or the analysis of process data. The modular software concept is based on Linux, Java apps and open interfaces. The configuration and handling is web-based, free from programming and performed logically in three simple steps.

Through targeted process monitoring in real time, failures and waste can be avoided, plant components can be automatically deactivated for energy efficiency or servicing can be planned proactively. The Rexroth IoT Gateway offers manufacturing companies of all sizes an opportunity to connect new and already existing machines simply and cost-efficiently to local condition monitoring solutions or MES systems, for example.

Robust hardware, modular software, open interfaces

The IoT Gateway hardware also fulfills the industrial requirements for an i4.0 upgrade with protection category IP20 for the control cabinet assembly. The software that runs on it is based on the Linux operating system. With the integrated Java virtual machine, the efficient deployment of the Java-based applications and corresponding cloud services is done via an OSGi framework. For quick commissioning, different Java apps for typical application scenarios are provided with the IoT Gateway. The user receives a detailed overview of the collected data of the "devices app" in real time via the web-based dashboard. Sensor and process values can then be pre-processed in the processing app and be forwarded to various IoT services, such as those from Bosch Software Innovations or Oracle, for data collection and analysis.

Plug-and-Run in three steps

The configuration and handling of the IoT Gateway is done quickly, conveniently and completely free of programming via the integrated web interface. In the first step, the sensors are selected and configured in the devices app, in the second step, the data is pre-processed in the processing app and in the third step sent to the superimposed systems. The supported range of sensors covers digital and analog interfaces based on the scaled I/O portfolio IndraControl S20, Bluetooth Low Energy, or USB and RFID.

Starter Kit – IoT Gateway and Production Performance Manager

The IoT Gateway is available as a stand-alone solution and as part of a Starter Kit. The Starter Kit contains in addition to the IoT Gateway the Production Performance Manager from Bosch Software Innovations. The software merges the collected information into one visualization and forwards specified events to defined persons. In this way, it can serve as the basis for efficient and comprehensive production control. Bosch Rexroth will present the IoT Gateway as part of its comprehensive complete portfolio for the first time at the SPS IPC Drives 2016 in Nuremberg under the motto "Connected Automation i4.0 now!".

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 31.100 associates generated sales revenue of approximately 5.4 billion euros in 2015.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 375,000 associates worldwide (as of December 31, 2015). The company generated sales of 70.6 billion euros in 2015. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing and sales network covers some 150 countries. The basis for the company’s future growth is its innovative strength. Bosch employs 55,800 associates in research and development at 118 locations across the globe. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.”

Additional information is available online at www.bosch.com , www.bosch-press.com , twitter.com/BoschPresse

 

Search press releases


Contact

Johanna Rauch
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1358
johanna.rauch@boschrexroth.de




Related Articles

2019-04-16
Press Information

Bosch Rexroth reports strong sales growth in fiscal 2018

In 2018, Bosch Rexroth generated a turnover of around €6.2 billion. This means the drive and control technology provider posted a 12.4% increase year-over-year. Adjusted for currency effects, growth was 13%. At the end of 2018, incoming orders amounted to €6.7 billion – a 3.8% increase over the positive previous business year.


2019-04-11
Press Information

Cast off for the journey into the future of industrial communication

Real-time wireless communication, full connectivity and interoperability from the field level to the cloud: these are all prerequisites for realizing the factory of the future. In order to actually make use of what is technically possible, all automation providers have to agree on an open standard from the field level to IoT communication. There has been great progress here: The Field Level Communication (FLC) initiative of the OPC Foundation for full interoperability of field devices is gaining momentum.