085-12 Lohr, 2012-11-27

Innovative machine concepts through new approaches in software engineering

Open Core Interface

With the Open Core Interface OEMs can develop application programs with Java as native apps and integrate smartphones seamlessly into the automation process.

Rexroth opens up more possibilities for OEMs thanks to enhanced access to the control core

When it comes to software engineering for machines and systems, OEMs are faced with new challenges. In addition to increased efficiency in PLC automation, they are increasingly interested in realizing customized software functions to set themselves apart from the competition. This is where integrating modern information technologies opens up new possibilities in production. IEC 61131-3-based engineering is reaching its limits here. Therefore, Bosch Rexroth is now using Open Core Engineering to connect PLC and IT automation and give developers a greater degree of freedom in software engineering. OEMs can flexibly access the control core of the system solutions IndraMotion MLC and IndraLogic XLC from applications based on high-level languages. This allows them to realize customized solutions independently and more easily, and at a lower cost than before.

Open Core Engineering brings the requirements from previously separated engineering worlds together in one integrated solution. At its center are software tools and function toolkits that build entirely on open standards and technologies. The new Open Core Interface enhances the software engineering – which until now has been focused on PLC automation – enabling it to work with applications based on high-level languages. With numerous function libraries which are adapted to different development environments it is now possible to have functions directly access the control core. This allows OEMs to realize customized software functions in-house and to integrate IT technologies based on high-level languages into their automation solutions. Specific examples are the integration of simulation tools or the use of smart devices with native apps. Moreover, the Open Core Interface makes it possible to integrate production machine functions and data out of IT-based applications such as management execution systems.

Access all the way to the core with various devices and programming languages

With the Open Core Interface, OEMs are free to choose their platform – PC, controller or smart device – and the required programming language: From C/C++, C# (.NET), Visual Basic, VBA (Office), LabView G, Objective-C and Java to all programming applications that support the integration of Microsoft COM libraries. They can even realize customized control functions for real-time applications independently of the control program. This means that the engineers can use high-level languages to write their own software functions which then run as low-level real-time application directly on the control, or in non-real-time on external devices such as PCs or smart devices. Now machinery manufacturers can realize innovative functions themselves - even those that require enhanced core access. This will also allow them to protect their know-how.

Smart devices and native apps as application examples

The Open Core Interface supports Apple iOS and Google Android, which are the two major operating systems for smartphones and tablets at this point. The high market penetration of smart devices combined with their innovative and comfortable operating concepts is generating a lot of interest with machinery manufacturers and operators. They are realizing that the future will bring new ways of making communication between humans and machines more user-friendly, flexible and intuitive. With the Open Core Interface, OEMs can develop application programs with Java as native apps, integrate smartphones seamlessly into the automation process, and support machine operators with new diagnostic and operating concepts. The native applications run entirely on the smartphone or tablet, so that the machine program remains untouched.

More efficient through integrated knowhow

Open Core Engineering combines these new degrees of freedom in software engineering with engineering efficiency from project planning to ongoing operations, which is what the market had been demanding. The IndraWorks software integrates all tools as well as Rexroth's industry and technology-specific know-how in the form of function toolkits in an integrated engineering framework. The GAT (Generic Application Template) software toolkit, for instance, automatically generates the executable machine program based on the developer's instructions, thereby laying the foundation for the development of modular machine software. Another example is the FlexProfile software toolkit. It simplifies the execution of complex machine functions by automatically adjusting all drive movements to changed parameters in the production process.

A variety of industry and technology-specific software toolkits speed up the engineering as OEMs receive already pre-made basic functions. Based on open standards such as sercos, OPC-UA or PLCopen, Open Core Engineering also provides certainty for the future and protects the investments of machinery manufacturers and operators.

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the Rexroth brand name, the company supplies more than 500,000 customers with tailored solutions for driving, controlling, and moving. Bosch Rexroth is a partner for Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies. The company provides customized solutions tailored to the needs and specifications of each individual market. As The Drive & Control Company, Bosch Rexroth develops, produces, and sells components and systems in over 80 countries. As part of the Bosch Group, Bosch Rexroth and its 34,900 associates generated approximately 5.1 billion euros in revenue in 2010.

To learn more, please visit

The Bosch Group is a leading global supplier of technology and services. According to preliminary figures, more than 300,000 associates generated sales of 51.5 billion euros in the areas of automotive and industrial technology, consumer goods, and building technology in fiscal 2011. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in some 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent more than 4 billion euros for research and development in 2011, and applied for over 4,100 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial.

Additional information can be accessed at ,


Search press releases


Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573