Press

Content
PI 052-16 Lohr am Main, 2016-12-13

Higher filtration effect and a longer service life

The fifth generation of filter materials by Rexroth protects hydraulic systems and reduces the operating costs

For failsafe operation of hydraulic systems, optimum filtration of the fluid is essential. 80 % of all failures can be traced back to contaminated fluid. The responsible particles are not visible to the naked eye. New filter media of the fifth generation by Rexroth reliably retain these contaminations. At the same time, they lower the operating costs thanks to a significantly increased service life of the filter elements. In addition, this is the first time a manufacturer has equipped all filter elements in standard sizes with an electrical conductive fleece filter medium by default. In this way, the risk of electric discharges in connection with zinc- and ash-free hydraulic oils is reduced.

Based on the extensive application experience as a world-leading manufacturer of hydraulic systems and with the help of recent insights of materials science and comprehensive flow analyses, Rexroth has developed completely new filter materials. The fifth generation is used in all Rexroth filter elements of all marketable sizes. The ideally coordinated filter systems made of glass fiber achieve high retention rates which is the measure for filter efficiency. These rates indicate at which ratio the filter element retains particles of a defined size. The ß-values of the new filter material according to ISO 16889 are far over 200 depending on the filter rating. In this way, users achieve very good filtering results and increase their system availability thanks to optimally cleaned hydraulic fluids.

Electrical conductive fleece in series

The newly developed filter elements are equipped with an additional conductive fleece filter medium by default. It provides for a charge exchange between oil and filter material and thereby reduces the risk of electrostatic charge and discharge in the filter. End users of hydraulic systems increasingly use zinc- and ash-free oils. These hydraulic media usually have reduced conductivity. If it is less than 300 picosiemens per meter, the danger of electrostatic discharge increases. Discharge processes are often visible in the form of lightning discharges or can be identified by a sizzling noise. Each discharge can burn tiny amounts of oil and reduce the service life of the medium. Discharges can also burn holes in the filter layers. This reduces the retention rate and increases the danger of particles passing through the filter and causing damage in the system.

Only two instead of three filter element exchanges

In addition to the high filtration efficiency, the new material also increases the dirt holding capacity. Compared to the previous generation, the new filter elements absorb up to 50 percent more particles and thereby prolong the service life by the same value under constant operating conditions. Over the operating time, three filter exchanges were required up to now. The new generation reduces the effort to two exchanges. This means that users save costs for filter elements, their disposal and the associated labor.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 31.100 associates generated sales revenue of approximately 5.4 billion euros in 2015.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 375,000 associates worldwide (as of December 31, 2015). The company generated sales of 70.6 billion euros in 2015. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing and sales network covers some 150 countries. The basis for the company’s future growth is its innovative strength. Bosch employs 55,800 associates in research and development at 118 locations across the globe. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.”

Additional information is available online at www.bosch.com , www.bosch-press.com , twitter.com/BoschPresse

 

Search press releases


Contact

Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de




Related Articles

2018-07-18
Statement

Steel, rubber and oil – digital?! Industrial hydraulics must pick up the pace on the way to the digital future

Industrial hydraulics – today, this largely amounts to standard hydraulics consisting of iron, rubber, oil and, maybe, 24V connection sockets. At the same time, Industry 4.0 and the Internet of Things are changing the face of the factory floor: Decentralized intelligence, integrated sensor technology and connectivity have already become key requirements for many industrial applications. Nonetheless, hardware-intensive industrial hydraulics is in a position from which it can smoothly glide into this new digital environment. The requirement: Hydraulic manufacturers must accept the challenge of intensively advancing digitalization.


2018-06-11
Press Information

Software of the future: Freed from …

…the restraints of hardware – the software of the future. In the factory of the future, machine modules and processing stations will be regularly reorganized, flexibly take on new tasks and retrieve the appropriate software function. This change has already begun: Machine manufacturers are already able to install identical control functions on various device platforms without any extra effort. Here is an overview of concepts for today and tomorrow: