, 2017-03-01

‘Lifting’ a 48,000-ton platform in the open ocean is no easy task

Picture: Pioneering Spirit

Special Bosch Rexroth components and control systems on board the ‘Pioneering Spirit’

It was the biggest assignment Bosch Rexroth in Boxtel had ever faced, and it took more than two years to carry it out. But they seized with both hands the opportunity to research and supply the hydraulic components and associated local controls for the innovative lifting system on board the Pioneering Spirit, conceived and developed by Allseas.

The request came from Allseas, an offshore specialist, or in fact from founder and owner Edward Heerema. A specially designed ship to lift entire offshore platforms off their piles in a single movement, for which Allseas had developed in-house a complete motion compensation system and associated control system. Allseas also wrote the software for the principle behind the motion system. Then they asked Bosch Rexroth to further develop the design of the hydraulics and the arrangement of specific components of these lifting beams, and to supply specialist hydraulic components and drive systems.

Ron van den Oetelaar, Managing Director of Bosch Rexroth Benelux, says: “We’d already worked closely with the Allseas engineers in Delft in the past, on other projects. So we had already supplied all sorts of components for special ships laying pipelines in the ocean. We were honored when Allseas gave us the engineering task of investigating the technical design for a new lifting system. It was a unique opportunity to display our technological knowhow. Working closely with the Allseas engineers, who developed the unique form and functionality of the ship and the principle of the lifting beams for the ‘topsides lift system’, our engineering team investigated various technical control options for the individual lifting beams. They looked at many different variations: hydraulic, electrical, and hybrid combinations of both technologies. The hydromechanics and electromechanics were a challenge, but so was the digital technology (controls, software, bus systems, etc.). Allseas wanted the ship to be able to handle platforms weighing up to 48,000 tons. That’s no easy task. Especially when you realize not only how accurately but also how fast it has to happen. During the development process countless tests were carried out and simulations performed so that, together with the engineers at Allseas, we could find the optimal solution. When after a couple of years’ development we had got it right ‘on paper’, we were given the job of manufacturing and supplying the hydraulic components and drive systems for the individual beams.

Enormous efficiency gains

It used to take ships with cranes and dozens of workers weeks or even months to construct or dismantle a platform piece by piece on the open ocean. “Pioneering Spirit”, 382 meters long and 124 meters wide, can lift the top section of a platform off its piles in 9 seconds. The motion compensation system is activated during preparations to pick up a platform. It consists of 16 lifting beams operated from the bridge of Pioneering Spirit. Using the lifting beams, a platform is raised 2.5 meters in a single swift movement so that the topsides of the platform becomes detached from the substructure. Then the ship moves away, and the topsides is carried towards the shore.

The technology applied in this situation by Allseas, also known as “swell compensation”, is exceptionally complex due in part to the simultaneous movements of the lifting beams along multiple axes.

Engineered to order

For this assignment, was it possible to use standard components from the Bosch Rexroth range, or were custom components required? “Standard components can rarely be used for special projects of this size,” Van den Oetelaar replies. “Apart from a few catalog components, such as valves and plunger pumps, most of the components and subsystems were developed specifically for this ship. This includes cylinders, control devices, generators, mounting plates, etc. The local digital control systems that we supplied for the lifting beams were also developed specifically for this assignment. That applies to both the control hardware and the software. During the design process, we made intensive use of powerful simulation tools to predict system behavior, finite element methods to compute critical parts and components for strength, and analysis techniques to identify risks in the process flow. But it’s always exciting when the first job gets underway. That took place last August, and involved lifting the 13,500-ton top section of the Yme platform, off the Norwegian coast. Everything worked perfectly. Since then, the remaining four lifting beams (including Bosch Rexroth components) have been installed on the ship for larger lifting jobs. It’s great that our designers, production staff, service engineers and other technicians have been able to make such an important contribution.”

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 31,100 associates generated sales revenue of approximately 5.4 billion euros in 2015.

To learn more, please visit

The Bosch Group is a leading global supplier of technology and services. It employs roughly 390,000 associates worldwide (as of December 31, 2016). According to preliminary figures, the company generated sales of 73.1 billion euros in 2016. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected industry. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to create solutions for a connected life, and to improve quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 450 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing, engineering, and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 120 locations across the globe, Bosch employs 59,000 associates in research and development.

Additional information is available online at,,,


Search press releases


Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573

Related Articles

Press Information

Intelligent hydraulics for increased availability

Connected hydraulics increase the availability of machinery and plants through condition monitoring and predictive maintenance. For this purpose, Rexroth offers scalable solutions, from individual units with local evaluation to the complete, cloud-based monitoring of large plants. Sensors measure all relevant operating conditions and software detects wear before it leads to failure. Retrofitting kits also economically integrate already installed plants into these concepts.

Press Information

Linear motion, short time to market

Stand-alone linear axes are the trend. The combination of electrical drive unit and mechanical or hydraulic cylinder reduces installation space and engineering time and combines our specific professional knowledge in one system. With ready-to-mount and i4.0-enabled solution packages, Bosch Rexroth is in line with the current market requirements regarding electrification, digitalization and monitoring as well as condition-based maintenance. The uniform control and drive concept which is used in the different technologies serves as a basis for a short time to market and the economical implementation of hybrid solutions.