Press

Content
PI 011-17 Lohr am Main, 2017-04-10

Electromechanical cylinders from Rexroth last up to 25% longer

EMC electromechanical cylinders from Rexroth set new benchmarks for service life and cost-efficiency.

Lower system costs thanks to longer service life

Rexroth has increased the service life of EMC electromechanical cylinders by up to 25% while retaining the same dimensions. This lowers life cycle costs and reduces maintenance effort for end users. The manufacturer has simultaneously reduced the minimum length of the cylinder and minimized the required installation space by up to 22%. This allows design engineers to create even more compact solutions.

The ready-to-install EMC electromechanical cylinders consist of anodized aluminum -housings in ISO standard dimensions with integrated ball screw drives. Thanks to continuously optimized production processes, Rexroth has significantly increased the load ratings of the ball screw drive core component and thus raised the nominal life of the electromechanical cylinder by up to 25%. Design engineers now have the option to use a smaller size with the same load, which allows them to reduce costs. Rexroth validated the new values in comprehensive stress and life cycle tests under various conditions of use.

At the same time the specialist for linear motion technology has lowered the minimum stroke of the cylinder in all sizes by up to 50%. In the smallest variant the minimum stroke that can be ordered is only 30 mm. Thanks to the shorter strokes that can now be selected, the required assembly space is reduced by up to 22%.

The ready-to-install, complete systems minimize the design and installation effort. Design engineers can put together their customized EMC variants in just a few steps on the Bosch Rexroth website. After selection and dimensioning in the new LinSelect tool, users switch to the online CAD configurator which takes over the configuration data. Registered users can then see the delivery time and price of the selected variants in the Rexroth eShop.

Electromechanical cylinders combine the advantages of an actuator - with the possibilities provided by digital control of electrical drives. Users can optimally adjust the complete solution to a wide range of applications thanks to a complete - product family with high variability. The EMC family from Rexroth consists of seven finely scalable sizes. The largest variant, EMC100-XC-2, has thrust forces of up to 56 kN. All versions can be ordered with a force measuring sensor on the end of the piston rod as well as on the timing belt side drive.

More details: www.boschrexroth.com/emc

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 31.100 associates generated sales revenue of approximately 5.4 billion euros in 2015.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 390,000 associates worldwide (as of December 31, 2016). According to preliminary figures, the company generated sales of 73.1 billion euros in 2016. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected industry. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to create solutions for a connected life, and to improve quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 450 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing, engineering, and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 120 locations across the globe, Bosch employs 59,000 associates in research and development.

Additional information is available online at www.bosch.com , www.iot.bosch.com , www.bosch-press.com , www.twitter.com/BoschPresse

 

Search press releases


Contact

Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de




Related Articles

2018-06-11
Press Information

Software of the future: Freed from …

…the restraints of hardware – the software of the future. In the factory of the future, machine modules and processing stations will be regularly reorganized, flexibly take on new tasks and retrieve the appropriate software function. This change has already begun: Machine manufacturers are already able to install identical control functions on various device platforms without any extra effort. Here is an overview of concepts for today and tomorrow:


2018-05-28
Press Information

Rexroth takes users on a digital journey of Linear Motion Technology

Instead of the previously strictly separate work steps in the dimensioning, configuration, start-up, actual use and diagnosis of Linear Motion Systems, Bosch Rexroth shows with a trade fair exhibit as a study the advantages of a continuous digital journey through the entire life cycle. Here, software tools and all individual pieces of information accompany the components and systems of Linear Motion Technology. At the Automatica 2018 trade fair, Bosch Rexroth is using a multi-axis system with its own intelligence as an example to present the entire range of production-ready and close-to-production digital solutions with which design engineers and users can react to changing conditions more quickly and flexibly than ever before.