International
 

Press

Content
PI 019-17 Lohr am Main, 2017-04-10

Linear system can handle welding spatter and chips

The sturdy CKK compact module with the "Resist" cover is unsusceptible to welding spatter and dry chip impact.

New in the product portfolio from Bosch Rexroth: the sturdy CKK linear motion axis with the "Resist" cover

Rexroth has now put the CKK compact module with the "Resist" cover, originally developed specifically for a European automobile manufacturer, into the linear motion technology standard product range. The ready-to-install linear motion axis is particularly suited for handling components during welding and dry chip impact. The new cover is free from paint-wetting impairment substances, PWIS. The connection dimensions, configuration and delivery times of the new series-produced variant correspond to the standard versions.

Welding applications always produce welding spatter, which can also hit the handling axes. It can also enter the interior of unprotected assemblies and lead to increased wear and premature breakdown. Therefore, the handling axes are often encapsulated, which causes high additional costs and poor accessibility. The CKK compact module with the "Resist" cover is different. Several hundred examples have been proving their worth for years in the body shop of a European automobile manufacturer. An additional plate with a toothed sealing profile prevents welding spatter and chips from entering the interior of the compact module. The exchangeable sealing profile consists of FKM material with a short-term temperature stability of up to 300 °C. The sealing profiles are silicone-free and therefore conform to PWIS. This is an important requirement of the automobile industry in order to guarantee the proper coating of components.

Apart from a slightly increased total height due to the additional profile, the CKK with "Resist" cover offered in sizes -110, -145 and -200 corresponds to the standard versions of the compact module with ball screw drive. It has an application-oriented long carriage with connection plate. The connection dimensions of the profile body and the carriage with connection plate are identical to those of the series. Thanks to the positive-locking connection technology with centering rings, no major adjustments are necessary during mounting and start-up.

The compact modules simplify motor attachment due to the locating feature and fastening thread. Design engineers configure the sturdy variants as usual with the online tools from Rexroth and maintain the corresponding CAD data. Adjustable switches across the entire travel path reinforce the high positioning accuracy and repeatability from the ball screw drive with zero-backlash nut system. The delivery times correspond to those of the standard compact module.

The CKK compact module with the "Resist" cover also fits into the one-point lubrication concept used in the automobile industry, for both liquid grease and oil. The sturdy linear motion systems are suitable for all handling applications relating to dry machining and welding of vehicles.

More details: www.boschrexroth.com/ckk

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 31.100 associates generated sales revenue of approximately 5.4 billion euros in 2015.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 390,000 associates worldwide (as of December 31, 2016). According to preliminary figures, the company generated sales of 73.1 billion euros in 2016. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected industry. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to create solutions for a connected life, and to improve quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 450 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing, engineering, and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 120 locations across the globe, Bosch employs 59,000 associates in research and development.

Additional information is available online at www.bosch.com , www.iot.bosch.com , www.bosch-press.com , www.twitter.com/BoschPresse

 

Search press releases


Contact

Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de




Related Articles

2019-10-07
Press Information

Installation space-saving linear axes for a wide range of handling tasks

The compact and ready-to-install MKK and MKR linear modules are now also available in the size 140. Featuring a sophisticated switching concept and an integrated measuring system, the new sizes also come readily prepared to be connected to central lubrication systems. The LinSelect engineering tool ensures that the linear modules can be selected and designed quickly and easily.


2019-07-08
Press Information

Additional sizes for Ball Screw Assemblies: The more dynamic way to achieve your goal

With quicker linear movements, machine manufacturers can increase productivity. With higher forces and precision requirements, the delicate interaction of the rotary speeds and torque of the electrical drive system with the size of the Ball Screw Assembly is crucial. With the four new sizes 8x5, 40x25, 40x30 and 50x30, Rexroth has further expanded its range of BASA Ball Screw Assemblies. With multi-start spindles and multi-start nuts, the load ratings and service lives of Ball Screw Assemblies are increased.