PI 023-17 Lohr am Main, 2017-05-16

IndraControl XM2201: Robust hardware for extreme environments

IndraControl XM for use in marine and offshore applications and in explosive atmospheres.

Rexroth’s controller is now certified for use on ships, offshore installations and in explosive atmospheres.

Six European and American certification boards have approved the IndraControl XM22 control hardware for use on ships and offshore installations even under extreme ambient conditions. The certifications include the control hardware, extension modules for the expansion of the communication interfaces as well as application-specific modules of the fast IndraControl S20 I/O portfolio. IndraControl XM is the latest powerful controller with IP20 protection. The XM embedded controller uses IEC 61131 compliant programming tools for PLC programs as well as motion control tasks to regulate electric, hydraulic and electro-hydraulic drives.

The environmental conditions on the high seas are already demanding enough, because the technology has to function simply, safely and reliably. This approach has been followed by classification societies for more than 150 years. Their task is to test the robustness and reliability of all components for shipbuilding and offshore operations. A specially optimized version of IndraControl XM, which is widely used in the industry, has now been certified by six classification societies for use on the high seas: the American Bureau of Shipping, Lloyd's Register, Bureau Veritas, Det Norske Veritas / Germanischer Lloyd, Registro Italiano Navale and the Federal Maritime and Hydrographic Agency. The modular and expandable control solution is also certified according to IECEx (protection class Ex ec IIC T4 Gc) for potentially explosive environments and is therefore also suitable, for example, for the switchgear application on oil and natural gas conveying devices.

Proven in extreme environments

This special variant of the IndraControl XM22 uses the same modern processor technology for high performance as the standard versions used in numerous stationary machine industries. The hardware proves itself as a high-performance solution even in applications with extreme ambient conditions, e.g. in metallurgy or wood processing in all climate zones. Selected S20 I/O modules are certified to complement the modular control system for a complete automation system. Application examples include winches, tank ballast systems or drill main drives and drill position handling.

The control modules are approved for an application temperature range from -25 to +60 ° C. The rugged and shock-resistant electromechanical system can withstand vibrational loads of up to 5 g and impacts of up to 30 g. Both the control electronics and the I/O modules are extremely resistant to EMC influences. The control system, on the other hand, has significantly reduced EMC radiation and thus minimizes effects on other devices in the control cabinet.

Open communication and easy commissioning

For the drive communication, IndraControl XM uses Sercos, a standardized real-time automation bus. Extension modules, which are registered by the certification companies, also extend the communication capabilities by providing data access through protocols such as CAN as master, PROFINET RT or Ethernet / IP as master or slave. This allows the control system to be integrated into the architecture on ships and offshore installations. In line with the high performance requirements at sea, Rexroth also offers certified servo drives of the IndraDrive ML family which cover a system power range of up to 4 MW. Electrohydraulic solutions from Rexroth use the same software kernels and automatically take into account the special features of fluid technology. With the fastest S20 modules currently available on the market, highly precise control of several synchronous hydraulic axes can be achieved. E.g. for hydraulic control of ship winches, hydraulic proportional valves can be controlled via certified S20 pulse width modules.

IndraControl XM reduces the commissioning times of the hardware and software to a minimum. The I/O modules are installed without tools with pluggable electronics. On the software side, technicians start the control via the First Touch user interface which requires only a standard internet browser.

Bosch Rexroth has a large presence in important maritime hubs as well as at the most important ports of international maritime shipping with service and spare parts capacities on site. The company has been equipping ships and offshore installations with drive and control technology for more than 50 years.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 29,500 associates generated sales revenue of approximately 5 billion euros in 2016.

To learn more, please visit

The Bosch Group is a leading global supplier of technology and services. It employs roughly 390,000 associates worldwide (as of December 31, 2016). The company generated sales of 73.1 billion euros in 2016. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected manufacturing. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 120 locations across the globe, Bosch employs some 59,000 associates in research and development.

Additional information is available online at , , , .


Search press releases


Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573

Related Articles

Press Information

DeepSea Mining Alliance visits Bosch Rexroth in Lohr

On April 27, 2017, the general meeting of the DeepSea Mining Alliance (DSMA) took place at Bosch Rexroth in Lohr. During a factory visit and dialog with experts beforehand, the participants could obtain information on products and solutions in the field of marine, offshore and subsea applications from Bosch Rexroth. As part of the event, Dr. Alexandre Orth, director of the marine and offshore sector at Bosch Rexroth in Lohr, has been elected as member of the board of DSMA. The other four newly elected members of the board of DSMA are Leonard Weixler, Heiko Felderhoff, Dr. Rudolf Bannasch and Dr. Steffen Knodt.

Press Information

Intelligent hydraulics for increased availability

Connected hydraulics increase the availability of machinery and plants through condition monitoring and predictive maintenance. For this purpose, Rexroth offers scalable solutions, from individual units with local evaluation to the complete, cloud-based monitoring of large plants. Sensors measure all relevant operating conditions and software detects wear before it leads to failure. Retrofitting kits also economically integrate already installed plants into these concepts.