International
 

Press

Content
PI 025-17 Lohr am Main, 2017-05-22

IndraDrive Mi: Independent universal talent with new cooling possibilities

Rexroth expands the range of applications of its IndraDrive Mi control cabinet-free drive system with additional cooling types for mains and supply modules.

Rexroth has already successfully moved the entire drive technology from the control cabinet to the machine. In addition to the IndraDrive Mi motor-integrated and motor-near drives, the company has developed decentralized supply and mains modules that allow machine manufacturers to install all electrical drive components directly on the machine. Now Rexroth has equipped these modules with new cooling options for a wide range of production environments and, in doing so, also expanded the range of applications.

The control cabinet-free IndraDrive Mi drive system allows for the realization of a completely independent drive solution. The supply unit that can be directly integrated into the machine makes this possible. Rexroth has now equipped these mains and supply modules with additional cooling options. Convection cooling and forced air cooling options are now also available in addition to the thermal interface for cold plate mounting or insulated mounting. These two types of cooling do not require any process water for cooling and allow for flexible use in a wide range of production environments. Applications for which no process water is available, such as in conveying or handling technology, in food and packaging technology or also to some extent in the printing and wood industry, do not require any additional recooling when using these new cooling options.

All mains connection components that were previously placed in the control cabinet are now realized in IP65 in the IndraDrive Mi and can be directly installed in the machine. The mains filter, mains choke and mains contactor are integrated in the KNK03 mains module to supply direct power from the grid. The regenerative KMV03 power supply module with control electronics, braking resistor and brake transistor has completely replaced the power supply and the control electronics in the control cabinet.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 29,500 associates generated sales revenue of approximately 5 billion euros in 2016.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 390,000 associates worldwide (as of December 31, 2016). The company generated sales of 73.1 billion euros in 2016. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected manufacturing. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 120 locations across the globe, Bosch employs some 59,000 associates in research and development.

Additional information is available online at www.bosch.com , www.iot.bosch.com , www.bosch-press.com , www.twitter.com/BoschPresse .

 

Search press releases


Contact

Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de




Related Articles

2019-11-26
Statement

Nowadays, mechanical engineering means software development

Nowadays, software development accounts for a significant part of the engineering work in mechanical engineering. Software tools from the world of IT are playing an ever greater role too. For machine manufacturers, software is valuable intellectual property. After all, it is a product of their know-how which helps to maximize the productivity of machines and systems. Through software, they stand out from the competition and can offer individual customer variants in a cost-effective manner. For machine users, being able to connect machines to their IT systems easily is becoming increasingly important. The communication capabilities of machine software are thus a key purchasing criterion.


2019-10-24
Press Information

A new world of automation

With the new ctrlX AUTOMATION platform, Bosch Rexroth has eradicated the traditional boundaries between machine control systems, IT and the Internet of Things. Centralized and decentralized automation topologies can now be created flexibly with the scalable platform. Thanks to a Linux real-time operating system, open standards, app programming technology, web-based engineering and a comprehensive IoT connection, ctrlX AUTOMATION reduces the engineering time and effort by 30 to 50%.