Press

Content
PI 027-17 Lohr am Main, 2017-06-06

Integrated absolute value measuring system with FANUC interface

Measuring system from Rexroth with interfaces to match the CNC controllers from Bosch Rexroth, Siemens and Fanuc.

IMS-A: robust, precise and simple at start-up

Bosch Rexroth, Siemens, FANUC: No matter which servo drive or controller the end user prefers, machine manufacturers can equip them all with no hassle - thanks to the measuring system IMS-A integrated into the linear guides. In addition to HIPERFACE*, SSI and DRIVE-CLiQ**, Rexroth now also provides an interface for FANUC automation systems. The absolute position measuring systems IMS-A are highly precise and resistant to metalworking fluids, all kinds of chips and electromagnetic interference fields.

Internationally active manufacturers of machine tools, 3D printers and related systems often provide their customers with the choice between two to three CNC controllers to cover regional preferences. While doing so, they follow a common-part strategy below the drive level as much as possible in order to reduce costs and complexity. Here, with the measuring system IMS-A integrated into the linear guides, Rexroth is opening up additional opportunities. As well as interfaces for CNC controllers from Bosch Rexroth and Siemens, IMS-A now also supports FANUC automation systems. With these variants start-up only takes a few minutes. With the Plug & Play encoder system, the person performing the start-up merely has to determine the respective zero point of the machine and the position offset. An electronic nameplate transfers all other information.

The absolute position measuring system integrated into the linear guides operates without contact and is therefore wear-free. Through its implementation in the runner block and the connected sealing concept, machine manufacturers can avoid energy-intensive air sealing systems, even in working areas with metalworking fluids, dust, chips and other contaminants. This means that the regular replacement or cleaning work that would usually be necessary for glass scales in these environments is no longer required. In a comprehensive series of tests, Rexroth has investigated the effect of a mixture of ferromagnetic laser cutting dust and grease lubricant on the scale. Almost all of the paste-like mixture was wiped away by the standard sealing lips of the runner block and the level of interference was so low in all of the tests that the specified accuracy was always met.

The measuring system is resistant to magnetic fields like those emitting/emitted from linear motors for example. Protected against vibrations and shocks, the sensors and evaluation electronics are placed in a housing on the end face of the runner block. Design engineers thus save the space for external measuring systems. Rail guides equipped with the IMS-A fit into existing machine designs without any constructional alterations in virtually every case. The absolute position is transferred with a resolution of 25 nm for all interfaces, while the repeatability is better than +/- 0.25 µm. The integrated scale is available at an accuracy of up to +/- 3 µm/m. With the IMS-A, users can implement several runner blocks on an up to 4,500 mm long profile rail independently and without any limitations on accuracy. The wear-free IMS-A does not require a battery for buffering the position. Even after a power failure, the measuring system still reports the exact position of the axis upon being switched on again from the integrated absolute scale without a homing cycle.

*HIPERFACE is a registered trademark of SICK STEGMANN GmbH.

**DRIVE-CLiQ is a registered trademark of Siemens.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 29,500 associates generated sales revenue of approximately 5 billion euros in 2016.

To learn more, please visit www.boschrexroth.de

The Bosch Group is a leading global supplier of technology and services. It employs roughly 390,000 associates worldwide (as of December 31, 2016). The company generated sales of 73.1 billion euros in 2016. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected manufacturing. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 120 locations across the globe, Bosch employs some 59,000 associates in research and development.

Additional information is available online at www.bosch.com , www.iot.bosch.com , www.bosch-press.com , www.twitter.com/BoschPresse .

 

Search press releases


Contact

Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de




Related Articles

2018-06-11
Press Information

Software of the future: Freed from …

…the restraints of hardware – the software of the future. In the factory of the future, machine modules and processing stations will be regularly reorganized, flexibly take on new tasks and retrieve the appropriate software function. This change has already begun: Machine manufacturers are already able to install identical control functions on various device platforms without any extra effort. Here is an overview of concepts for today and tomorrow:


2018-05-28
Press Information

Rexroth takes users on a digital journey of Linear Motion Technology

Instead of the previously strictly separate work steps in the dimensioning, configuration, start-up, actual use and diagnosis of Linear Motion Systems, Bosch Rexroth shows with a trade fair exhibit as a study the advantages of a continuous digital journey through the entire life cycle. Here, software tools and all individual pieces of information accompany the components and systems of Linear Motion Technology. At the Automatica 2018 trade fair, Bosch Rexroth is using a multi-axis system with its own intelligence as an example to present the entire range of production-ready and close-to-production digital solutions with which design engineers and users can react to changing conditions more quickly and flexibly than ever before.