, 2017-08-23

The ‘Next Generation Gangway’ at work in the Irish Sea

Photo: Barge Master and Bosch Rexroth’s motion-compensated gangway: ‘walk-to-work’ (Photo Credit: Bosch Rexroth)

Barge Master and Bosch Rexroth’s ‘Next Generation Gangway’ is in operation on the subsea-support walk-to-work vessel VOS Start from Vroon Offshore Services.

The ship is chartered by MHI Vestas Offshore for the installation of wind turbines at the Walney Extension Wind Farm at the Irish Sea. To make VOS Start one of the most innovative ships in the market a unique solution was provided by Barge Master and Bosch Rexroth, its partner for the gangway. The gangway is designed and built to the highest standards and certified under the new DNV-GL rules for motion-compensated gangways.

The unique Next Generation Gangway

The motion-compensated gangway is mounted on a height-adjustable pedestal with an integrated elevator enabling a continuous workflow. Additionally, the pedestal makes it possible for the gangway to land on any height, keeping the gangway horizontal and providing stepless transfers. Both people and cargo can be transported from the ship deck or the level below to the level of the gangway, where they can instantly cross.

The gangway has been extensively tested onshore at a specially designed test facility at Bosch Rexroth in Boxtel. The onshore testing made sure that only a very short period was needed to get the gangway operational on the VOS Start. Only a few days of offshore testing where needed. This next generation gangway, which is operated by a single operator, is equipped with extremely fast sensors and control technology. Movements of the ship can be translated into ‘counter movements’ of the gangway within milliseconds. Because of this the system is able to compensate for wave heights up to 3 meters (Hs) allowing safe transfers.

Making the system truly unique is the fact that forces are also measured in the tip of the gangway, which allows for the forces to be kept low. This reduces the possibility of the tip to slip, significantly increasing the workability.

Successful partnership

Barge Master is a leading company in the field of motion compensation systems. Its CEO, Martijn Koppert, explained that the partnership with Bosch Rexroth, the drive and control company, was not a coincidence. “We have been in business with Bosch Rexroth already since 2008. We started in a conventional supplier/customer relation, but this has evolved since the development of the Next Generation Gangway. We formed a Joint Project Team, which results in a far better system by using the best expertise available. This is proven by the fact that this gangway is an entirely new concept.”

The two Dutch companies worked in a close cooperation, using each other’s strengths. As stated by Martijn Koppert, “With this solution users are able to transfer people and goods from ship to platform 24 hours a day, 7 days a week, making this solution far better than anything available at the market at this moment. I am confident that, together with Bosch Rexroth, we will optimally serve the offshore wind market with this next generation gangway.”


Vroon Offshore Services is delighted to be operating this Next Generation Gangway. Foppe Molenaar, Vroon Newbuilding Superintendent states, “VOS Start is an ultramodern and state-of-the-art subsea-support walk-to-work vessel, providing clients with a totally new concept that offers optimum safety and comfort. By introducing this vessel – the first of its kind and one of two sister vessels constructed in China for Vroon – our Company aims to revolutionise working practices in the renewable energy and oil & gas sectors.

“The continuous access is what makes this system unique compared to traditional systems. The motion-compensated gangway system ensures safe and efficient transfer of personnel, whatever the sea conditions. These gangways are now the preferred option during construction and maintenance work at offshore windfarms and oil & gas platforms, offering clients a reliable and cost-effective alternative to helicopter flights. “It took just a two-month window to complete the final production of components, factory testing, on-board installation and commissioning, have the system fully certified, in operation and deployed in the windfarm. With this combination of fine facts we strongly believe that VOS Start can truly create a game-changing market!”


Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 29,500 associates generated sales revenue of approximately 5 billion euros in 2016.

To learn more, please visit

The Bosch Group is a leading global supplier of technology and services. It employs roughly 390,000 associates worldwide (as of December 31, 2016). According to preliminary figures, the company generated sales of 73.1 billion euros in 2016. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected industry. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to create solutions for a connected life, and to improve quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing, engineering, and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 120 locations across the globe, Bosch employs 59,000 associates in research and development.

Additional information is available online at , , , .


Search press releases


Vincent Stahlecker
5281 RV Boxtel NL
Phone: +31 411 651 682

Related Articles

Product Information

Focus on upgrade and retrofit of hydraulic systems

Blue Offshore, a rental company for specialized cable laying equipment, approached Bosch Rexroth from Boxtel, to increase the pulling force of the hydraulic cable tensioner and to upgrade and modernize the complete hydraulic installation.

Press Information

Highly wear resistant cylinder rod coating for industrial and civil engineering applications

The highly wear resistant Enduroq 1 coating is aimed at civil engineering and industrial applications. Enduroq 1 is based on a laser cladding technology developed in cooperation with the Fraunhofer institute, Europe's largest application-oriented research organization.