PI 037-17 Lohr am Main, 2017-09-18

Valuable data from the machine tool

The IoT Gateway from Rexroth makes machine tools transparent and provides a knowledge base for higher plant efficiency and more flexible processes.

The IoT Gateway from Bosch Rexroth allows machine data to be analyzed and evaluated in order to increase plant efficiency

  • Connect new and existing machines quickly and easily
  • Create transparency – without interfering with the existing automation
  • Live demonstration at the booth: status visualization of machine hydraulics

Both the users and manufacturers of machine tools are very keen to collect sufficient machine data in order to visualize and optimize the manufacturing processes and plant efficiency. The subsequent analysis of this data will reduce unplanned downtimes and lead to more efficient production with smaller batch sizes. With the IoT Gateway, Rexroth provides an easy to configure solution to collect sensor and machine data from existing, even older machinery and transfer it to higher-level IT systems. In terms of investment protection, this does not require any interference in the existing automation infrastructure.

To fulfill the increasing demand for flexibility in production, users and mechanical engineers are called on to connect the production processes beyond company boundaries and build flexible value creation networks from reliable machines and lines. Because the typical lifecycles of existing plants can be fifteen years or more, an extensive replacement investment is usually out of the question. High expenditure and interference in the automation infrastructure are two arguments against retrofitting existing drive and control technology. The IoT Gateway is a quick and cost-efficient alternative to this, which makes connecting plants simple and transparent.

Efficient IoT connection for new and existing plants

With the IoT Gateway, machine tools from different manufactures connect to the industrial Internet of Things and Services (IoT) in no time and without any programming effort. The user just need to select the parameters and sensors to monitor and configure the data transfer via the intuitive web-based interface. This system of sensors, software and IoT-capable industrial hardware is quick and easy to set up, handle and manage. Where necessary, data from existing control systems can be read out regardless of the manufacturer without intervening in the existing control project.

Finally, the user determines which data to process from the IoT Gateway and send to the higher-level systems to be monitored and evaluated. These could be databases, MES systems, operating and machine data logging systems or IoT cloud platforms from Bosch, Oracle or Microsoft, for example. In combination with the data analytics server from Rexroth, it provides an attractive system solution from a single source.

Typical application scenarios in machine tools

A common usage scenario for the IoT Gateway is the predictive maintenance of main spindles on older machine tools. Using additional oscillation and temperature sensors, impending failure can be recognized early on, meaning that crucial production components can be systematically exchanged. Missing information can also be gathered from the machine hydraulics without interfering in the plant software. For example, the current flow can be calculated from the signal designation of the hydraulic units.

As part of a live demonstration at EMO 2017, Bosch Rexroth will visualize the practical application of the IoT Gateway and data analytics server in connection with CytroPac, a small power unit, and a hydraulic cylinder.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 29,500 associates generated sales revenue of approximately 5 billion euros in 2016.

To learn more, please visit

The Bosch Group is a leading global supplier of technology and services. It employs roughly 390,000 associates worldwide (as of December 31, 2016). The company generated sales of 73.1 billion euros in 2016. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected manufacturing. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 120 locations across the globe, Bosch employs some 59,000 associates in research and development.

Additional information is available online at , , , .


Search press releases


Manuela Kessler
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-4145

Related Articles


The factory of the future creates added value through flexibility and agility

In future production environments demands on adaptability will rise. This development can only be realized by separating hardware and software in automation. Bosch Rexroth AG promotes this development primarily with a broad product spectrum from sensors to drive and control technology to software solutions.

Press Information

Connected Automation without limits

How can machine builders increase the Overall Equipment Effectiveness (OEE) and make use of machine data analytics for development, sales and service? Bosch Rexroth answers questions like these with a new i4.0 showcase, which among other things connects machines of Pfiffner, the leading global manufacturer of rotary transfer machines, and a production facility. The live demo also shows that "Connected Automation" has no technological limits. Because with its showcase Bosch Rexroth connects not only electrical components but also hydraulics and linear motion technology. The relevant software for condition-based monitoring and maintenance is formed by the new Data Analytics Server (DAS) and the IoT Gateway. A secure connection to the Bosch IoT Cloud allows performance monitoring across different locations.