Press

Content
PI 047-17 Lohr am Main, 2017-09-25

New welding control generation PRC7000 from Rexroth: reliable and efficient

The new welding controls PRC7300 and PRC7400 from Rexroth

Maximum quality for welding all sheet thickness combinations from steel through aluminium

Process safety and the highest quality at the welding spots are the core requirements for welding processes in the automotive and household appliance industry. With the new welding control family PRC7000, Rexroth has further improved its proven control and monitoring concept. New software tools and the modular structure increase availability and simplify operation through reduced commissioning times. The use of the latest semiconductor technology reduces energy consumption by up to 80 percent. With numerous interfaces for commonly used communication protocols, the controller also fits into the networked production environments of the future.

The new welding control generation PRC7000 with the PRC7300 for steel and projection welding, as well as the PRC7400 for aluminum spot welding and applications with the highest power requirements distinguish themselves through high availability and a modular design. The adaptive control algorithms of the PRC7000 assure a reproducible and high welding spot quality for welding the most diverse sheet thicknesses, from steel through aluminum. In addition, the adaptive process control and monitoring methods have already been designed for future material combinations in the welding process.

Networkable for Industry 4.0

The PRC7000 welding controls are prepared for horizontal and vertical networking in Industry 4.0 environments. Users can physically separate the welding PC and the user interface from the welding cell. The multi-processor architecture - for process control and communication - increases the data transfer rate without repercussions on the welding process control. The controller exchanges data with higher-level systems over all standard Ethernet real-time protocols and is WLAN-capable. The integrated webserver also allows wireless operation and diagnosis of the controller with smartphones or tablet PCs.

Commissioning accelerated by 90 percent

New software tools and the modular design of the systems reduce commissioning and changeover times by up to 90 percent. An application layer integrated as standard allows fast and targeted adaptation to the robot interface. An internal real-time bus is available for the connection of electric servo-gun and peripherals. The servo-gun front-end reduces the installation effort and enable the preventive maintenance of the welding gun. With open interfaces for the process, robot integration and communication, the entire system fits into a wide range of automation structures up to Industry 4.0 environments.

The new PRI7000 software for the commissioning, operation and diagnosis controls multiple welding controllers with one piece of hardware. It simplifies operation with intuitive Windows and web-based applications. New communication interfaces reduce the response and waiting times. The control saves up to 10,000 welding programs and thus fits well into a multi-variant production process.

Energy-efficient and compact

The new power electronics of the PRC7000 reduce power loss. This allowed the developers to use smaller sized coolers. The compact size is 30 percent smaller than that of the previous generation. Simultaneously, the new controller increases energy efficiency. It uses up to 30 percent less energy during welding, and up to 50 percent less energy at idle. The superior controller can switch the welding controllers into the standby mode during production breaks and then reactivate them again via the fieldbus protocol.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 29,500 associates generated sales revenue of approximately 5 billion euros in 2016.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 390,000 associates worldwide (as of December 31, 2016). The company generated sales of 73.1 billion euros in 2016. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected manufacturing. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 120 locations across the globe, Bosch employs some 59,000 associates in research and development.

Additional information is available online at www.bosch.com , www.iot.bosch.com , www.bosch-press.com , www.twitter.com/BoschPresse .

 

Search press releases


Contact

Manuela Kessler
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-4145
manuela.kessler@boschrexroth.de




Related Articles

2018-08-08
Statement

The digital journey of Linear Motion Technology has begun

While many mechanical engineers are still marveling at the force of which information technologies are making their way into factories, the basic technologies are also changing virtually unnoticed. To take Linear Motion Technology as an example, many still consider it a purely mechanical affair; however, more recent developments paint an entirely different picture. Matthias Rommel, Head of the Linear Motion Technology Business Unit at Bosch Rexroth AG explains which opportunities are now available due to digitization.


2018-04-23
Press Information

Bosch Rexroth presents collaborative robot based on KUKA

Bosch Rexroth continues to expand its portfolio of Automatic Production Assistants (APAS): With the APAS assistant, the company now also integrates KUKA technology into its product range. Unique product features enable a simple and safe entry into the world of human-robot collaboration. Complete with capacitive sensor skin to avoid collisions, selectable control and the widely-used PLC interface mxAutomation, the six-axis robot is set to become the perfect link for combining the strengths of human and machine in the factory of the future.