International
 

Press

Content
PI 052-17 Lohr am Main, 2017-10-09

The next generation of Linear Modules: fit for one-point lubrication and challenging applications

Comprehensive lubrication concept and consistent resistance to media: Revised MKK and MKR Linear Modules meet the tougher requirements of machine construction.

MKK and MKR Linear Modules from Rexroth with new functionalities

The third generation of MKK and MKR Linear Modules from Rexroth provides a considerably expanded range of equipment options for the familiar space-saving dimensions of the previous series. The ready-to-install linear axes are ready to be connected to the one-point lubrication systems. In the corrosion resistant versions, hard chrome plated ball screw drives and ball rails ensure a high resistance to chemicals.

The Linear Module consists of an anodized aluminum profile body with integrated ball rails and the option of a ball screw drive or a belt drive. Rexroth provides both drive types in the new generation, initially in sizes 65, 80 and 110. They are interchangeable with previous versions in the same dimensions and do not require large constructive adjustments. As ready-to-install assemblies, Linear Modules reduce the construction and installation effort in all types of machines and systems.

Rexroth addresses the industry-wide trend of automating maintenance work with one-point lubrication systems and thus increasing the life of the axes with a comprehensive lubrication concept. The corresponding components, ball screw drive and runner block are ready for one-point lubrication with liquid grease or oil. If the user is using their own lubricants, they can order the corresponding Linear Module components with only corrosion prevention and complete the initial lubrication for start-up by themselves. In the standard version, the manufacturer delivers the Linear Module with initial lubrication for ready to use.

In applications where increased corrosion resistance is required, the hard chrome plated ball screw drive, profiled rails and runner block resist NR can permanently withstand water and aggressive chemicals. Stainless-steel band covers with a new magnet profile enhance this resistance to media and increase the resistance to coolant/lubricants for example.

Rexroth delivers the ball screw drive variant of the Linear Module in lengths up to 5,400 mm. A screw support prevents vibrations at high rotational speeds from 4,000 mm onwards, and thereby increases the application window for highly dynamic uses. The Linear Modules with belt drive are available in lengths up to 9,400 mm.

The absolute measurement system IMS-A can be integrated into the modules in sizes 080 and 110. At the system start, it captures the exact position of the axis carriage directly and without a homing cycle. Using the incremental measuring principle, the IMS-A operates wear-free and is immune resistant to contamination and electric fields.

A new switch concept simplifies assembly and saves time. The magnetic field sensors for limit switches fit directly into the profile frame without additional mounting accessories so that no interfering contours are created. This means that the space-saving design is also retained in practice.

Two carriages with variable centerline-to-centerline distance also accommodate larger attachments with increased system rigidity. Centering holes in the carriages and frame simplify assembly because the use of centering rings produces a form-fitting connection and thus the adjustment work is substantially simplified.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 29,500 associates generated sales revenue of approximately 5 billion euros in 2016.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 390,000 associates worldwide (as of December 31, 2016). The company generated sales of 73.1 billion euros in 2016. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected manufacturing. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 120 locations across the globe, Bosch employs some 59,000 associates in research and development.

Additional information is available online at www.bosch.com , www.iot.bosch.com , www.bosch-press.com , www.twitter.com/BoschPresse .

 

Search press releases


Contact

Manuela Kessler
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-4145
manuela.kessler@boschrexroth.de




Related Articles

2020-09-21
Press Information

Successful transformation: from individual components to smart mechatronic solutions

Over the past three decades, Bosch Rexroth’s portfolio of ready-to-install linear axes has been further developed on an ongoing basis. In response to customer requirements, it now focuses on electrification and connectivity. With today’s linear motion technology components in combination with sensors, electronics and software, the company now offers mechatronic solutions for the Factory of the Future too.


2020-08-12
Press Information

Calculation program for Linear Motion Technology with new functions and greater ease of operation

Since 2008, the Linear Motion Designer has been the first choice when it comes to calculating and dimensioning Rexroth Linear Motion Technology components – and it is being improved all the time. The latest version of the software tool also allows you to dimension linear bushings and, thanks to new functions, enables you to do so even more quickly and conveniently. The Linear Motion Designer is thus an important part of Rexroth’s digital engineering and procurement chain.