PI 056-17 Lohr am Main, 2017-11-28

Flexible, robust, easy to connect: Industrial PCs from Rexroth

The scalable IPC platform meets customer-specific requirements for low to middle power ranges, in a particularly economical and future-proof manner.

The new generation of the industrial PC platform impresses with its low overall cost, good scalability and long service availability.

  • Scalable: the right model for every performance requirement
  • Cost effective: good price/performance ratio, maintenance-free design
  • Future-proof: Application of hardware until at least 2027

With new generation PR, VR, DR industrial PC platform, Bosch Rexroth sets new standards in the low and middle power range in terms of cost-effectiveness. Moderate acquisition costs, maintenance-free design and use of the hardware until at least 2027 combine an attractive price/performance ratio with investment protection. Equipped with up-to-date Intel processors from different performance classes, the box and panel PCs of the PR and VR series open up a well graduated system for a wide variety of tasks, including Industry 4.0 applications with high data throughputs. The modern multi-touch displays of the DR series are available for visualization and operation of the box PCs. As a special service, Bosch Rexroth also offers individualized designs, e.g. with the imprint of the OEM logo.

The PR box PCs are suitable for either horizontal or vertical installation. For demand-oriented visualization and operation, the high-resolution capacitive multi-touch widescreen displays of the DR series are available in graduated sizes from 12 to 21 inches. They can be connected either via DisplayPort/USB or CDI+, where up to three multi-touch displays can be connected without repeaters with just one cable up to 100 meters long. The VR panel PCs combine the properties of PR and DR in one unit and primarily target HMI-based applications.

High economic efficiency and investment protection

Bosch Rexroth uses various Intel CPUs with different performance levels in order to achieve incremental scalability. The range extends from the quad-core ATOM processor with 1.6 GHz to the multi-core i7 processor with 2.6 GHz. In addition to the needs-oriented selection of CPUs, the maintenance-free, EMC, shock and vibration-proof design also makes a positive contribution to cost-effectiveness. Since the solution does not use fans or other moving parts, energy efficiency and long-term availability are increased. In addition, Bosch Rexroth guarantees that the hardware will be in use until at least 2027. The series will be available for at least five years, followed by a further five years in which Rexroth will provide service and spare parts.

Connectivity and data security

Users can choose from a variety of expansion options and numerous interfaces to customize connectivity according to their needs. They range from WLAN / Bluetooth, Gbit LAN/, RS-232 and RS-422/485 to 4G with LTE/HSPA+/GPRS and GPS, up to 16 digital inputs and 8 digital outputs. In addition, hardware extensions with half-size PCIe and full-size mini PCIe slots are possible. High-performance, robust and RAID-capable SSD memories from 32 GB increase system availability and data backup, especially with regard to documentation tasks for traceability of all process steps.

Ready for Industry 4.0

For networked environments and data-intensive i4.0 tasks, all new models feature cycle-synchronous Intel i210 chipsets. They form the basis for real-time-capable Ethernet communication with controllers or higher-level systems in order to make production more flexible or shorten cycle times. The TPM 2.0 modules for security-by-design, which are also installed throughout the system, are used for secure, non-manipulable operation of the industrial PCs from the boot process through to the running application as well as for the internal storage of certificates, keys and other protective mechanisms.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 29,500 associates generated sales revenue of approximately 5 billion euros in 2016.

To learn more, please visit

The Bosch Group is a leading global supplier of technology and services. It employs roughly 390,000 associates worldwide (as of December 31, 2016). The company generated sales of 73.1 billion euros in 2016. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected manufacturing. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 120 locations across the globe, Bosch employs some 59,000 associates in research and development.

Additional information is available online at , , , .


Search press releases


Manuela Kessler
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-4145

Related Articles

Press Information

Flexible, continuous production

The growth markets of energy storage and printed electronics are characterized by considerable pressure in terms of time, quality and costs. Bosch Rexroth positions itself as an incredibly reliable automation partner, delivering easy-to-integrate system solutions to handle the current challenges in the printing, semiconductor and display industry. For example, the flexible transport system FTS suitable for vacuum applications and the precision motion control MPC accurate to the nanometer demonstrate how roll-to-roll, coating and production processes can be continuously optimized and made future proof.

Product Information

Software drives innovation

Vertical and horizontal connectivity, digital engineering, economic production of very small batch sizes – without software, these core characteristics of Industry 4.0 would be inconceivable. Even today, software contributes a great deal to the added value created by machines, while in the factory of the future it supplies the necessary intelligence for modular, mobile and connected production components. Using its Connected Automation portfolio, Bosch Rexroth will be demonstrating how state-of-the-art software affects competitiveness and time-to-market at the SPS IPC Drives.