International
 

Press

Content
PI 057-17 Lohr am Main, 2017-11-28

Connected automation across the board

At SPS IPC Drives, Bosch Rexroth will present the complete spectrum of automation and electrification - from entry into the industrial IoT, to requirement-specific IPCs and intelligent drive solutions

At SPS IPC Drives, Bosch Rexroth presents the latest expansion of its Connected Automation range.

  • Comprehensive: Range of automation and electrification solutions
  • Connected: IoT Gateway V2 with enhanced features and new hardware
  • Cost-efficient: Industrial PCs set standards
  • High-performance: Expanded range of motors for intelligent drive systems
  • Innovative: Version 14 of CNC and Motion-Control system software

With the latest expansion of the Connected Automation range, Bosch Rexroth will introduce six comprehensive solution programs at the SPS IPC Drives. The IoT Gateway software V2 allows for tailor-made introduction to the IoT for both new and existing machines. The PR, VR, DR industrial PC platform supplies cost-efficient hardware power for increasingly complex control tasks. The drives solution area presents new drive options including single-cable servo motors with ATEX-conformity and Safety on Board. The CNC system MTX offers advantages for machining and forming. In the Motion Control area, visitors can experience the new version of the Motion-Control system MLC with new functions for robotics, PLC and machine safety and the vacuum-compatible Flexible Transport System FTS.

Within the PLC (Programmable Logic Control) and IoT solution program, Bosch Rexroth shows how both new and existing machines can become efficient, purposefully transparent and connected. The IoT Gateway software V2 offers many new connectivity options for this purpose, including the wireless connection of Bosch XDK and CISS sensors or recording controller data via OPC DA and other third-party control systems such as Beckhoff CX and Allen Bradley/Rockwell ControlLogix. In addition to the high-performance embedded control XM from Rexroth, industrial PCs are also available as hardware options – particularly the new IPC generation PR based on Linux – with WiFi, USB and HDMI interfaces, among other things. The Device Portal – a joint development by Rexroth and Bosch Connected Industry – makes it possible to centrally and securely manage distributed infrastructures as well as setup, configuration and remote maintenance.

The industry PC generation PR, VR, DR meets the increased hardware requirements for more complex tasks, including i4.0. The range of box and panel PCs and displays, which are scalable for lower and medium power ranges, sets new standards with their new processors in terms of software functionality, connectivity and flexibility. Additionally, minimal investment costs and maintenance-free design improve cost efficiency. In addition, Bosch Rexroth guarantees that the hardware will be in use until at least 2027.

Bosch Rexroth’s drive range for middle strength is completed by the self-cooled, iron-core linear motors ML3. The high-torque synchronous servo motor MS2N addresses demanding tasks with SafeMotion, with an integrated encoder in the SIL3 PLe category. The MS2E series with ATEX conformity according to device group II, category 3G/3D, is suitable for environments with explosive gases and dusts.

For the CNC systems, the new version 14 of the MTX provides functions for machining, forming or 3D printing. With up to 60 independent channels, 250 simultaneously controlled axes and full OPC-UA server/client functionality, it sets the global benchmark for the shortest PLC and CNC cycle times and i4.0 communication.

The new version 14 of the Motion-Control system MLC controls over 1,000 synchronized drives within microseconds and to nanometer precision, when required. It offers an extensive Motion Library for machines and processes, as well as full connectivity for IoT, Multi-Ethernet, I/O, Vision and third-party solutions. Other innovations include the high-performance embedded control YM and the vacuum-suitable Flexible Transport System FTS. The FTS is intended for a range of applications such as mounting and handling, battery production and semiconductor production. Furthermore, Bosch Rexroth presents its market-leading control for resistance welding.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 29,500 associates generated sales revenue of approximately 5 billion euros in 2016.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 390,000 associates worldwide (as of December 31, 2016). The company generated sales of 73.1 billion euros in 2016. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected manufacturing. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 120 locations across the globe, Bosch employs some 59,000 associates in research and development.

Additional information is available online at www.bosch.com , www.iot.bosch.com , www.bosch-press.com , www.twitter.com/BoschPresse .

 

Search press releases


Contact

Manuela Kessler
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-4145
manuela.kessler@boschrexroth.de




Related Articles

2020-11-24
Press Information

Now available for everyone: Compact control platform ctrlX CORE from Bosch Rexroth

Bosch Rexroth has defined the industrial control system of the future with its compact ctrlX CORE control system. With its open and flexible architecture, the control platform removes the boundaries between the IPC, embedded system and drive-based technology platforms. This scalable “all-purpose control system” offers numerous advantages such as a fewer component requirement and a reduced engineering effort as well as higher productivity. The embedded control system is now available in series production.


2020-11-05
Press Information

Bosch Rexroth at the SPS Connect: Rethinking in automation required

With its ctrlX AUTOMATION platform, Bosch Rexroth is exploring completely new avenues in automation and is bringing together control technologies, IT and the IoT to create an open, scalable system. The company will demonstrate how this works at the virtual SPS Connect trade fair from 24 to 26 November 2020. Here, Bosch Rexroth will present the automation platform with its latest innovations in the areas of services, safety solutions, I/O modules and its own ecosystem. The compact control platform ctrlX CORE is also available for purchase just in time for the trade fair.