Press

Content
PI 060-17 Lohr am Main, 2017-11-28

Software drives innovation

Industry 4.0 would be inconceivable without software. The Connected Automation portfolio from Bosch Rexroth demonstrates its full potential in terms of connectivity and time-to-market.

With innovations in its Connected Automation portfolio, Bosch Rexroth demonstrates the importance of software in automation.

  • Scalable: universal software, needs-based hardware
  • Connectable: High connectivity thanks to open architecture and i4.0 standards
  • Standardized: Unification of the control platforms
  • Efficient: Fast engineering thanks to function toolkits, templates and wizards

Vertical and horizontal connectivity, digital engineering, economic production of very small batch sizes – without software, these core characteristics of Industry 4.0 would be inconceivable. Even today, software contributes a great deal to the added value created by machines, while in the factory of the future it supplies the necessary intelligence for modular, mobile and connected production components. Using its Connected Automation portfolio, Bosch Rexroth will be demonstrating how state-of-the-art software affects competitiveness and time-to-market at the SPS IPC Drives.

Characteristic of Rexroth software in all areas is open architecture with Open Core Interface, which allows direct access to control functions and lays the foundation for highly efficient engineering. That's because controllers, drives and peripherals can be consistently and uniformly configured and controlled within the intuitively designed IndraWorks software environment – based on current Windows technologies and comprehensive wizards. Thanks to various function modules and templates, standard applications can be created simply by parameterizing. State-of-the-art tools and languages are available for explicit programming. The virtual commissioning of machines and plants makes testing safer and shortens the time-to-market. The automation solutions from Bosch Rexroth are becoming IoT-ready thanks to the integrated i4.0 standard OPC-UA.

In the field of CNC systems, the new version 14 of the MTX provides new capabilities for multi-technological machining with up to 60 channels and 250 axes. A variety of standard applications is already prepared, including bending, turning, milling, grinding, punching/nibbling, jet cutting or rotary transferring. Innovative functions make even industrial 3D printing useful for series production of small batch sizes. Customer-specific functions can also be added via the open architecture.

Version 14 of the Motion-Control system MLC from Bosch Rexroth also contains considerable potential for standardization in addition to many prepared standard applications. Because it includes ready-to-use function toolkits for robotics, PLC, safety and integrated servo functions, in addition to comprehensive motion control, which means the control platforms for packaging, production and other industries can be standardized. For complex applications, the Generic Application Template (GAT) function toolkit reduces engineering efforts by up to 60 percent by automatically generating modular machine programs based on the IEC 61131-3 and PLCopen PLC standards. With the CamBuilder function toolkit electronic cams can be graphically created and simulated. After the successful simulation, the function blocks for the control are automatically generated, thereby greatly reducing errors in the manual creation process.

A further innovation in the Connected portfolio is that function toolkits, such as the Open Core Interface, allow PLC (Programmable Logic Control) to become ILC (IoT Logic Control). The IoT-enabled PLC system ILC version 14 addresses special machine construction, logistics plants and general automation and connects them easily and highly connectively with the Internet of Things. In addition to Sercos, ProfiNET and EthernetIP, ILC software version 14 continues to feature a new EtherCAT softmaster for controlling I/O components.

Like the MLC and ILC software, the IoT Gateway V2 is purely software based and can therefore not only be used on the embedded control XM but also on industrial PCs, for example on the new PR generation of IPCs from Bosch Rexroth. In addition to connectivity, the software is also crucial for cross-site manageability – with the IoT Gateway, the new device portal – a joint development by Rexroth and Bosch Connected Industry –allows for centralized and secure management of distributed infrastructures.

The drive system software MPx20 also contributes to fast and cost-optimized new machine development. It permits continuous connectivity within the 100 W to 4 MW power range, integrates safety and intelligence functions such as vibration damping, and accelerates the development and testing of control programs thanks to drive-internal axle simulation.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 29,500 associates generated sales revenue of approximately 5 billion euros in 2016.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 390,000 associates worldwide (as of December 31, 2016). The company generated sales of 73.1 billion euros in 2016. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected manufacturing. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 120 locations across the globe, Bosch employs some 59,000 associates in research and development.

Additional information is available online at www.bosch.com , www.iot.bosch.com , www.bosch-press.com , www.twitter.com/BoschPresse .

 

Search press releases


Contact

Manuela Kessler
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-4145
manuela.kessler@boschrexroth.de




Related Articles

2018-12-11
Press Information

Avoiding the traps: The five biggest stumbling blocks in the introduction of IIoT

Industry 4.0, the Industrial Internet of Things or the factory of the future: More and more industrial users are thinking about digitalizing their manufacturing operations. There is no magic formula to this transformation. But you also do not have to make every possible mistake along the way.


2018-06-11
Press Information

Software of the future: Freed from …

…the restraints of hardware – the software of the future. In the factory of the future, machine modules and processing stations will be regularly reorganized, flexibly take on new tasks and retrieve the appropriate software function. This change has already begun: Machine manufacturers are already able to install identical control functions on various device platforms without any extra effort. Here is an overview of concepts for today and tomorrow: