International
 

Press

Content
PI 003-18 Lohr am Main, 2018-02-06

Rexroth offers digitalization of analog interfaces in hydraulics via IO-Link

Low connection costs for components thanks to M12 connector and electronic name plate.

Additional connection for bi-directional communication in parallel to field bus

Reduced connection costs at increased availability: Rexroth harnesses the advantages of the IO-Link open standard also for hydraulic actuators and sensors. As of now, 4WRPEH proportional control valves and HEDE10 pressure switches are available with IO-Link interfaces. Connection is realized via the decentralized and quick IP67 I/O system S67E IO-Link Master. This offers users direct access to the field bus and all data provided by the actuator/sensor.

Industry 4.0 is often much closer than we think: While individual suppliers present their own solutions for networking of machine peripherals and better utilization of data, there are already now established and open standards that offer the same. IO-Link is supported by around 150 companies and enables digital communication of peripherals with control in parallel to common field buses. With proportional valves and pressure switches, Rexroth now includes the first hydraulic actuators and sensors into the network. This way, the specialist in the field of hydraulics promotes the integration of fluid technology in Industry 4.0 applications as IO-Link enables vertical connection of components all the way into IT systems.

IO-Link standardizes and simplifies wiring thanks to standard M12 connectors with unshielded 3-conductor/5-conductor cables. This way, extensive time and fault-intensive individual wiring per hand is no longer required. Project planning of devices is realized with the engineering tool of the respective PLC manufacturer. All blocks for communication are freely available for the IoT-ready PLC systems ILC and Motion Control systems. In combination with IndraWorks Engineering, they enable direct access to project planning, parameterization and testing. The parameters can always be adjusted to new conditions.

The standardized electronic name plate of plug & play devices reduces machine and system standstill. By means of authorized remove control, servicing operations are enabled to access and evaluate operating conditions like temperature, operating hours and error status during running production for predictive maintenance concepts. This way, wear and system errors can be recognized before failure and machine standstill. The respective devices with servicing requirements are localized and displayed. Thanks to IO-Link, devices can also be replaced by personnel without special training. Components are clearly identified via site ID and electronic name plate for easy replacement by interchangeable components. Parameterization is carried out automatically by the IO-Link Master without any need for action by the technician. This way, replacement of components can be ensured without causing any problems.

Following the 4WRPEH proportional valve and the HEDE10 pressure switch, Rexroth intends successive fitting of additional hydraulic actuators and sensors with IO-Link interfaces to complete their product range.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 29,500 associates generated sales revenue of approximately 5 billion euros in 2016.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 400,500 associates worldwide (as of December 31, 2017). According to preliminary figures, the company generated sales of 78 billion euros in 2017. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected industry. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to create solutions for a connected life, and to improve quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing, engineering, and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 125 locations across the globe, Bosch employs 62,500 associates in research and development.

Additional information is available online at www.bosch.com , www.iot.bosch.com , www.bosch-press.com , twitter.com/BoschPresse .

 

Search press releases


Contact

Manuela Kessler
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-4145
manuela.kessler@boschrexroth.de




Related Articles

2022-10-25
Press Information

Primary-controlled press drive: Simply more efficient

With the SHP4V primary-controlled press drive from Bosch Rexroth, machine manufacturers can simplify their hydraulic constructions significantly and speed up commissioning. The servo-hydraulic pump units which can be mounted on the manifold significantly improve energy efficiency and reduce noise emissions.


2022-10-25
Press Information

Die cushion control system with proven safety

With the new IH04 Type E standard modules from Bosch Rexroth for the die cushion function, engineers can work with the most common switching systems. Thanks to the standardized safety concept with a DGUV test certificate, the modules meet general safety requirements with minimal outlay. They can optionally be combined with an energy recovery function which reduces the energy consumption of the die cushion module at the same time.