International
 

Press

Content
PI 014-18 Lohr am Main, 2018-06-05

Bosch Rexroth expands additive manufacturing

3D printing processes support versatile production

Versatile production of hydraulic components with 3D printing process

  • Joint project with TRUMPF and Heraeus Additive Manufacturing
  • Printed servo valves are lighter, more compact and more energy efficient
  • Customer-specific variants can be produced at short notice

The topic of additive manufacturing is becoming increasingly important in the production of small series and prototypes, as well as in the area of Industry 4.0. Bosch Rexroth also believes in this future-oriented technology. The company worked with TRUMPF and Heraeus Additive Manufacturing to develop a further additive manufacturing process for the cost-effective production of hydraulic components. With a focus on the Selective Laser Melting method, the project involved the production of servo valves. As an additional standard procedure to conventional production this can be used above all for quick production of small batch sizes and customized variants. Bosch Rexroth already uses several 3D printers for the production of casting cores for control blocks in Lohr and has expertise in the entire process chain from engineering to 3D printing to the finished product.

Thanks to the wealth of options at the component level, hydraulics offers a high degree of freedom in configuring tailor-made drive solutions. However, this diversity increases costs for manufacturers in production. The use of the Selective Laser Melting 3D printing method reduces the level of complexity. It enables quick and economical production of servo valves or spools for directional control valves at the smallest of batch sizes. In a joint project with TRUMPF and Heraeus Additive Manufacturing, Bosch Rexroth's manufacturing specialists developed the entire process chain: from design that has been optimized for 3D printing to the finished product.

Printed variants are significantly lighter and more compact than conventionally manufactured designs. Optimized passageways reduce throttle losses and increase energy efficiency. In the future, designers will also be able to integrate new functions into the components. In the course of the project, the project team developed hybrid manufacturing of servo valves for future series applications. As part of this Rexroth combined traditionally machined preforms with 3D printed components. As a further element, the project team tested the printing of hollow cylinders as spools for directional control valves.

The project used the TRUMPF TruPrint 5000. In the TruPrint 500, three 500-watt TRUMPF fiber lasers work simultaneously on a workpiece. This cuts the printing time for a servo valve almost in half. TRUMPF also covers the entire additive manufacturing process chain, including parts and powder management.

Heraeus Additive Manufacturing supported the project by selecting the most suitable materials and is working on the flow behavior of the steel powder and particle size distribution in the range of 20 to 40 μm. In comparison: a human hair has a diameter of about 100 µm. Only reliably high powder quality makes reproducible component quality possible under real production conditions. The compressive strength of the servo valves printed so far corresponds to those of the milled components of the same steel.

Bosch Rexroth has been using the 3D printing process involving sand molds for the production of cast cores for control blocks for several years. As a result, even single units and prototypes can be manufactured with extremely short lead times. This enables customers to significantly reduce the time-to-market for their solutions and quickly implement customer-specific variants.

As one of the world’s leading suppliers of drive and control technologies, Bosch Rexroth ensures efficient, powerful and safe movement in machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation. It enables fully connected applications with intelligent components, tailored system solutions, and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology and linear motion and assembly technology, including software and interfaces to the Internet of Things. With locations in over 80 countries, more than 30,500 associates generated sales revenue of 5.5 billion euros in 2017.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 400,500 associates worldwide (as of December 31, 2017). According to preliminary figures, the company generated sales of 78 billion euros in 2017. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected industry. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to create solutions for a connected life, and to improve quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiaries and regional companies in some 60 countries. Including sales and service partners, Bosch’s global manufacturing, engineering, and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 125 locations across the globe, Bosch employs 62,500 associates in research and development.

Additional information is available online at www.bosch.com , iot.bosch.com , www.bosch-press.com , twitter.com/BoschPresse .

 

Search press releases


Contact

Manuela Kessler
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-4145
manuela.kessler@boschrexroth.de




Related Articles

2020-11-20
Press Information

Linear power made easy

Bosch Rexroth’s development work has taken the hydraulic linear drive to a whole new level. The evolutionary CytroForce concept manages to squeeze previously bulky structures into a smart compact axis for power, movement and positioning tasks. The out-of-the-box solution consisting of flow-optimized standard modules sets new benchmarks in terms of power density, energy efficiency and quiet operations. It is supplied as a plug-and-produce system, meaning that even machine manufacturers who do not possess expertise in hydraulics can benefit from the optimized overall costs involved.


2020-09-12
Press Information

Green hydraulics for climate protection

Climate protection initiatives or the EU’s Green Deal are increasing the pressure on machine manufacturers to help their customers achieve their targets with energy-efficient hydraulic solutions. Compared to conventional technologies, the Sytronix variable-speed drives from Bosch Rexroth reduce energy consumption and electricity costs by up to 80 percent. The intelligent electrohydraulic systems indirectly reduce CO2 emissions by the same amount. Bosch Rexroth obtained these figures during real modernization projects.