International
 

Press

Content
, 2018-12-11

Avoiding the traps: The five biggest stumbling blocks in the introduction of IIoT

Industry 4.0, the Industrial Internet of Things or the factory of the future: More and more industrial users are thinking about digitalizing their manufacturing operations. There is no magic formula to this transformation. But you also do not have to make every possible mistake along the way. Bosch Rexroth now has more than five years of experience in the introduction of Industry 4.0, experience it gained in its own operations and in other companies as well. In the process, the company’s automation specialists have identified the five biggest stumbling blocks that complicate the job of introducing IoT and drive up its costs.

1. No planning: collecting data without any payoff

Data is the raw material of connected manufacturing and continuous improvement. So far, so good. But users allow themselves over and over again to be talked into using vast numbers of sensors and collecting billions of bits of data that are then evaluated by a standard software in the world of IT. The problem: The standard software does not recognize specific machines and processes and churns out only seemingly relevant results. To really know what information counts, employees must be brought into the process and be given an opportunity to share their knowledge and experience. The first way to increase transparency in all processes is the visualization of information. Working in a closed-loop process, employees can identify the really important findings and optimize the measurement process. Experience has shown: Focusing on manufacturing is hardly enough. Rather, holistic approaches also add information about logistics, purchasing, development and all other company functions.

2. Thinking too big: wanting to achieve everything at once

Some users try to do it all in one fell swoop by introducing Industry 4.0 during one major project and smoothing out all of the wrinkles at the same time. This is an iffy approach because it will tremendously increase complexity. As a result, it will become difficult to directly determine cause and effect. In addition, this approach frequently leads to overinvestment because it quickly creates the impression that the digital transformation can be achieved only with new systems and machines. An approach that involves many small steps has proven itself to be the most effective. During pilot projects, effects can be specifically determined and optimized during brief closed loops. At the same time, this process gradually introduces employees to the topic and gains their support. These pilot projects frequently demonstrate that available machines and systems can be easily connected later and can continue to be used – a step that saves time and money.

3. Wrong foot: Using an incorrect standard

Some machine manufacturers and end users prematurely select a standard for the future. That’s thoughtless because the world of standards for Industry 4.0 is in constant motion. The only sure thing is change itself. A future-focused machine connection must not only meet all current standards, but also must be able to be easily modified in response to future changes. Users can protect their past investments only through openness and flexibility.

4. Reinventing the wheel: programming everything yourself

You’ll find them in many companies: the tinkerers who come up with tailored, gold-trimmed solutions for internal purposes. But this is a risky proposition. This approach consumes huge amounts of both money and time. Simply writing the documentation for a proprietary solution takes up a tremendous amount of time, not to mention the fact that standard solutions are much more user friendly. With the help of these solutions, users can connect machines within a few hours and centrally manage all IoT devices in their network. One other very important finding: Mixing machine and IoT functions in a machine control system results in unnecessary complexity. Security and certification reasons will restrict updating options. For this reason, it makes more sense to operate IoT functions on dedicated systems and to concentrate on real-time communications between the systems.

5. Nothing will happen: dismissing security

These numbers are frightening: In surveys, more than half of responding companies acknowledge that they do not feel prepared to fend off attacks launched against their IoT devices. 94 percent said they even expected their vulnerability would grow. They are right, too! There are proven IT security processes that can be quickly and seamlessly extended to production, such as network segmentation and firewalls. Particularly helpful: instruments with which users can centrally manage all IoT devices and simultaneously install security updates at all locations around the world. This step protects connected manufacturing operations, and users can focus on their real jobs with a clear conscience.

As one of the world’s leading suppliers of drive and control technologies, Bosch Rexroth ensures efficient, powerful and safe movement in machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation. It enables fully connected applications with intelligent components, tailored system solutions, and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, gear technology and linear motion and assembly technology, including software and interfaces to the Internet of Things. With locations in over 80 countries, more than 30,500 associates generated sales revenue of 5.5 billion euros in 2017.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 402,000 associates worldwide (as of December 31, 2017). The company generated sales of 78.1 billion euros in 2017. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected manufacturing. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, crossdomain solutions from a single source. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiary and regional companies in 60 countries. Including sales and service partners, Bosch’s global manufacturing, engineering, and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 125 locations across the globe, Bosch employs some 64,500 associates in research and development.

Additional information is available online at www.bosch.com , www.iot.bosch.com , www.bosch-press.com , www.twitter.com/BoschPresse .

 

Search press releases


Contact

Johanna Appel
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1358
johanna.appel2@boschrexroth.de




Related Articles

2019-04-16
Press Information

Bosch Rexroth reports strong sales growth in fiscal 2018

In 2018, Bosch Rexroth generated a turnover of around €6.2 billion. This means the drive and control technology provider posted a 12.4% increase year-over-year. Adjusted for currency effects, growth was 13%. At the end of 2018, incoming orders amounted to €6.7 billion – a 3.8% increase over the positive previous business year.


2019-04-11
Press Information

Cast off for the journey into the future of industrial communication

Real-time wireless communication, full connectivity and interoperability from the field level to the cloud: these are all prerequisites for realizing the factory of the future. In order to actually make use of what is technically possible, all automation providers have to agree on an open standard from the field level to IoT communication. There has been great progress here: The Field Level Communication (FLC) initiative of the OPC Foundation for full interoperability of field devices is gaining momentum.