International
 

Press

Content
PI 010-19 Lohr am Main, 2019-02-19

APAS inline assistant: Continuous material flow without safety fence

For an optimal process flow, the APAS inline assistant enables integrated logistics solutions with product tracking. This makes it easy to automate and optimize process flows.

HRC-capable robot makes space-saving and transparent logistics possible

  • Collaborative robot closes the gap between automated guided vehicles (AGV) and transfer systems in the line
  • Space-saving automation
  • Intelligent material flow optimizes process flows

Space-saving automation with free access to all machines: These are the current challenges facing intralogistics. To meet these requirements, manufacturers are looking for compact solutions that can accommodate many machines in the tightest of spaces while being easily accessible. With its collaborative robot with no safety fence, the APAS inline assistant, Bosch Rexroth offers an essential element for automated, integrated logistics solutions with product tracking. The integrated camera means parts are reliably recorded and gripped, thus guaranteeing the secure flow of goods.

The APAS inline assistant is a robot integrated into the assembly line, which operates without the need for a safety fence. Thanks to its unique contact-free safety technology, this robot, which has been available since January 2018, is predestined for human-robot collaboration (HRC): Production material is fed manually or automatically using shuttles. With its integrated camera, the robot arm can also detect parts that have not been perfectly fed in, grasp them correctly and place them on a conveyor belt or on a trolley with blister stacks. Bosch Rexroth thus makes continuous material flow possible and closes the gap between its new ActiveShuttle autonomous transport system and its versatile transfer systems. Thanks to its compact design, the robot arm takes up little space and is ideally suited to supplementing or extending existing systems, even if the logistics operations were not originally designed for automation.

Space-saving automation with a high level of safety

The robotic arm is integrated into manufacturing without a protective fence or enclosure and avoids collisions with its sensor skin at performance level d, category 3. Thanks to its large switching distance and the contact-free detection of people, the robot reaches a safe speed of 0.5 m/s. The optional far range monitoring feature, using a laser scanner for example, is mounted at a height of 90 cm to 1.10 m and reliably detects employees at a greater distance. This allows the operating speed of the robot to be increased up to 2.3 m/s. For logistics and production planners, who are now required to add robots to existing hall layouts and machine concepts, this means that the environment hardly needs to be changed at all.

Intelligent material flow for Logistics 4.0

For intelligent material flow, the APAS inline assistant can be logistically connected in such a way that makes Track and Trace possible. The integrated camera records, for example, the product code and a higher-level system informs the robot on which goods carrier and on which conveyor the product should be placed in order to proceed through different production steps.

As one of the world’s leading suppliers of drive and control technologies, Bosch Rexroth ensures efficient, powerful and safe movement in machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation. With its intelligent components, customized system solutions and services, Bosch Rexroth is creating the necessary environment for fully connected applications. Bosch Rexroth offers its customers hydraulics, electric drive and control technology, gear technology and linear motion and assembly technology, including software and interfaces to the Internet of Things. With locations in over 80 countries, more than 30,500 associates generated sales revenue of 5.5 billion euros in 2017.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 410,000 associates worldwide (as of December 31, 2018). According to preliminary figures, the company generated sales from operations of 77.9 billion euros in 2018. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected manufacturing. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiary and regional companies in 60 countries. Including sales and service partners, Bosch’s global manufacturing, engineering, and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 125 locations across the globe, Bosch employs some 69,500 associates in research and development.

Additional information is available online at www.bosch.com , www.iot.bosch.com , www.bosch-press.com , www.twitter.com/BoschPresse .

 

Search press releases


Contact

Manuela Kessler
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-4145
manuela.kessler@boschrexroth.de




Related Articles

2019-03-31
Press Information

Additive manufacturing: From a niche existence to series production

Additive manufacturing has made the successful journey from research labs to prototypes and small-batch production. A broad range of manufacturing companies are now printing their own spare parts or individual special components. The technology is now about to take its next development step, a move that is designed to introduce it into series production. It faces a number of huge challenges along the way, including: Up to now, the technology has not been connected to the automated world of manufacturing. Through the development partnership between BigRep and Bosch Rexroth additive manufacturing will to tap its full potential for the factory of the future.


2019-03-31
Press Information

First aid in case of machine downtime

By allowing wireless access to the error memory of all machines equipped with Rexroth control systems, the new Digital Service Assistant (DSA) app from Bosch Rexroth makes it easy for end users to obtain help whenever servicing is required. It clearly identifies components and allows spare parts to be ordered or repairs to be made out more quickly. As a modular building block, OEMs can fully integrate the app into their service concepts.