International
 

Press

Content
PI 050-19 Lohr am Main, 2019-10-16

Twice as strong but still compact

Frame size MS2N13 expands the performance range of Bosch Rexroth synchronous servo motors.

Frame size MS2N13 expands the performance range of Bosch Rexroth synchronous servo motors.

New synchronous servo motor with frame size MS2N13 from Bosch Rexroth extends upper performance range

 

With twelve new variants of the synchronous servo motor MS2N, Bosch Rexroth is expanding the performance range of the engine series at the high end. With up to 692 Nm, the maximum torque is almost doubled. These new, compact motors offer high continuous power and an extended speed range to manufacturers.

Bosch Rexroth has increased the continuous power within the small installation space through optimized electromagnetic design and use of the reluctance effect to create torque. The new frame size MS2N13 comprises four compact lengths in three cooling variants each: Self-cooling, forced-ventilated or water cooling. With a continuous torque of up to 345 Nm and maximum speeds of up to 3,600 rpm, they are particularly suited for powerful applications in plastics processing machines, in forming technology or in heavy-duty machining.

The motor series MS2N is a true all-rounder for all applications in automation and combines dynamics with compact dimensions and maximum energy efficiency. The motors can be configured flexibly, with a wide range of shafts, encoders and holding brakes to choose from. Designers can select them in line with the respective requirements. The integrated SafeMotion encoders with the high performance class SIL3/PLe make additional safety components in the machine redundant.

The encoders interact with drive controllers to work as sensors and collect the operational data of the axis. This way, the motors are integrated in the increasingly networked field level of the future. MS2N also play an integral part in maximizing productivity in the new Bosch Rexroth Automation world, ctrlX AUTOMATION.

As one of the world’s leading suppliers of drive and control technologies, Bosch Rexroth ensures efficient, powerful and safe movement in machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation. With its intelligent components, customized system solutions and services, Bosch Rexroth is creating the necessary environment for fully connected applications. Bosch Rexroth offers its customers hydraulics, electric drive and control technology, gear technology and linear motion and assembly technology, including software and interfaces to the Internet of Things. With locations in over 80 countries, more than 32,300 associates generated sales revenue of roughly 6.2 billion euros in 2018.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 410,000 associates worldwide (as of December 31, 2018). The company generated sales of 78.5 billion euros in 2018. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT company, Bosch offers innovative solutions for smart homes, smart cities, connected mobility, and connected manufacturing. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to deliver innovations for a connected life. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 460 subsidiary and regional companies in over 60 countries. Including sales and service partners, Bosch’s global manufacturing, engineering, and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At nearly 130 locations across the globe, Bosch employs some 68,700 associates in research and development.

Additional information is available online at www.bosch.com , www.iot.bosch.com , www.bosch-press.com , www.twitter.com/BoschPresse .

 

Search press releases


Contact

Manuela Kessler
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-4145
manuela.kessler@boschrexroth.de




Related Articles

2019-11-26
Statement

Nowadays, mechanical engineering means software development

Nowadays, software development accounts for a significant part of the engineering work in mechanical engineering. Software tools from the world of IT are playing an ever greater role too. For machine manufacturers, software is valuable intellectual property. After all, it is a product of their know-how which helps to maximize the productivity of machines and systems. Through software, they stand out from the competition and can offer individual customer variants in a cost-effective manner. For machine users, being able to connect machines to their IT systems easily is becoming increasingly important. The communication capabilities of machine software are thus a key purchasing criterion.


2019-10-24
Press Information

A new world of automation

With the new ctrlX AUTOMATION platform, Bosch Rexroth has eradicated the traditional boundaries between machine control systems, IT and the Internet of Things. Centralized and decentralized automation topologies can now be created flexibly with the scalable platform. Thanks to a Linux real-time operating system, open standards, app programming technology, web-based engineering and a comprehensive IoT connection, ctrlX AUTOMATION reduces the engineering time and effort by 30 to 50%.