International
 

Press

Content
PI 024-20 Lohr am Main, 2020-10-02

Bosch Rexroth sets new standards for safe automation with ctrlX SAFETY

The fastest and most compact safety solution on the automation market

  • Scalable: From a drive-integrated solution to complete safety control
  • Efficient engineering through graphical programming
  • Compact design, fastest reaction time and flexible use

With ctrlX SAFETY, Bosch Rexroth introduces a novelty to the automation market: the most responsive and compact safety solution of its kind. The scalable system can be used as required – from the drive-integrated SafeMotion solution in ctrlX DRIVE to the complete ctrlX SAFETY control. In addition to the flexible use, the advantages include a very high level of safety thanks to the fastest reaction times and efficient engineering through graphical programming of the safety PLC.

ctrlX SAFETY is based on two components that can be used independently or as an overall system: SafeMotion and SafeLogic. The hardware is extremely compact and, as a safety control, its graphical programming allows the required programs to be created quickly and easily without extensive training. The intuitive engineering interface, a documentation-supported user guidance and ready-made dialogs for the acquisition of acceptance-relevant information enable significantly faster engineering than conventional solutions. For more demanding applications, the hardware can be extended by additional I/O modules via the safe fieldbus. It has flexible interfaces such as digital I/O, ctrlX SAFETYlink, Safety over EtherCAT (FSoE) and PROFIsafe (in preparation). The exchange of safe I/O signals between the safety control and the SafeMotion on the ctrlX DRIVE is performed via ctrlX SAFETYlink.

SafeMotion is based on the modular drive system ctrlX DRIVE and has a scalable software. It is available as an entry-level version, with extended functions or for the highest requirements. “SafeMotion brings safety functions exactly where the motion occurs: to the drive. It is therefore unmatched in speed. At the same time, this system allows a purely drive-based safety solution to be implemented completely independently of the higher-level control system,” explains Steffen Winkler, Vice President Sales of the Business Unit Automation & Electrification Solutions at Bosch Rexroth.

Compact, lightning fast and adaptable – but safe

The overall result is the fastest and most compact safety solution on the market. ctrlX SAFETY is also characterized by its high adaptability. Steffen Winkler explains: “As a complete solution, SafeMotion and SafeLogic communicate via our ctrlX SAFETYlink. With it, a 5-10 times faster reaction than with safety-oriented protocols via classic field buses is possible. Together with local I/Os, the shortest processing times of 1 ms in the FastChannel task contribute to this. These features form the basis for highest protection and the compact design of safety devices.”

ctrlX SAFETY allows for machine integration in the smallest installation space (thanks to shortened reaction times) and the integrated certified safety technology enables efficient machine acceptance. Once a safety solution has been planned, it can be integrated into different machine concepts without complex adaptation. As it supports the most common safe fieldbus protocols, ctrlX SAFETY can be integrated into almost any automation system, and modular safety strategies with safe cross communication can be realized.

“The user thus receives a solution tailored to his individual safety requirements with maximum flexibility and safety. The use of open standards and safe connectivity at all levels and the fast and versatile selection of safety functions complies with the principle of our open, integrated automation platform ctrlX AUTOMATION. ctrlX SAFETY enhances this established platform as a trend-setting safety system,” says Steffen Winkler.

As one of the world’s leading suppliers of drive and control technologies, Bosch Rexroth ensures efficient, powerful and safe movement in machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, and Factory Automation. With its intelligent components, customized system solutions and services, Bosch Rexroth is creating the necessary environment for fully connected applications. Bosch Rexroth offers its customers hydraulics, electric drive and control technology, gear technology and linear motion and assembly technology, including software and interfaces to the Internet of Things. With locations in over 80 countries, roughly 31,000 associates generated sales revenue of roughly 6.2 billion euros in 2019.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. It employs roughly 400,000 associates worldwide (as of December 31, 2019). The company generated sales of 77.7 billion euros in 2019. Its operations are divided into four business sectors: Mobility Solutions, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT provider, Bosch offers innovative solutions for smart homes, Industry 4.0, and connected mobility. Bosch pursuing a vision of mobility that is sustainable, safe, and exciting. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to facilitate connected living with products and solutions that either contain artificial intelligence (AI) or have been developed or manufactured with its help. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 440 subsidiary and regional companies in 60 countries. Including sales and service partners, Bosch’s global manufacturing, engineering, and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. Bosch employs some 72,600 associates in research and development at 126 locations across the globe, as well as roughly 30,000 software engineers.

Additional information is available online at www.bosch.com , www.iot.bosch.com , www.bosch-press.com , www.twitter.com/BoschPresse .

 

Search press releases


Contact

Manuela Kessler
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-4145
manuela.kessler@boschrexroth.de




Related Articles

2020-10-01
Press Information

With ctrlX SERVICES, Bosch Rexroth is expanding its wide range of support services for ctrlX AUTOMATION

Bosch Rexroth is expanding its ctrlX AUTOMATION platform by adding new services for users: App Store, Device Portal and online Community. The platform with app technology stands out with its open, modular design and opens up entirely new possibilities in the field of industrial automation. ctrlX SERVICES docks onto the platform and makes life much easier for developers.


2020-10-01
Statement

Automation means software development

When we launched ctrlX AUTOMATION at the end of 2019, we said from the outset that mechanical engineering nowadays means software development. We are now going a step further and saying that automation means software development. Why?