International
 

Press

Content
Lohr am Main, 2022-09-12

Plastics sector pioneers sustainable drive concepts

Guido Hettwer, Head of the Business Unit Industrial Hydraulics, Bosch Rexroth AG

Manufacturers of plastics machines are traditionally pioneers for new drive concepts which improve performance and energy efficiency. Variable-speed pump drives for example were first installed on a large scale in injection molding machines. The first electrohydraulic drive systems for controlled gap adjustment and closing movements were used in extrusion and blow molding machines.

Nowadays, modularly interchangeable hydraulic, hybrid and electric drive concepts are used in plastics machines to cater for different requirements in a flexible manner. At the same time, hydraulic systems offer clear advantages when it comes to power density and robustness, especially in higher performance classes. Modern hydraulics is also increasingly connected and flexible and works with great energy efficiency.

As a result, variable-speed pump drives in hydraulic power units and self-contained actuators reduce energy consumption by up to 80 percent. Optimized components reduce the amount of materials used, while hydraulic manifolds produced using 3D sand core printing allow a free choice of shapes and a reduction in pressure losses.

Flexible drive solutions with a short time to market are required if machine manufacturers are to produce smaller batches economically. During the design phase, online selection and configuration tools as well as preconfigured mechatronic modules significantly reduce engineering times. Simulations improve design quality as regards movement times and accuracy, control and aperture design. Software wizards guide users quickly through the commissioning process. Machine development and commissioning times are reduced as a result.

 

Search press releases


Contact

Manuela Kessler
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-4145
manuela.kessler@boschrexroth.de




Related Articles

2017-04-24
Press Information

Intelligent hydraulics for increased availability

Connected hydraulics increase the availability of machinery and plants through condition monitoring and predictive maintenance. For this purpose, Rexroth offers scalable solutions, from individual units with local evaluation to the complete, cloud-based monitoring of large plants. Sensors measure all relevant operating conditions and software detects wear before it leads to failure. Retrofitting kits also economically integrate already installed plants into these concepts.


2017-04-24
Press Information

Linear motion, short time to market

Stand-alone linear axes are the trend. The combination of electrical drive unit and mechanical or hydraulic cylinder reduces installation space and engineering time and combines our specific professional knowledge in one system. With ready-to-mount and i4.0-enabled solution packages, Bosch Rexroth is in line with the current market requirements regarding electrification, digitalization and monitoring as well as condition-based maintenance. The uniform control and drive concept which is used in the different technologies serves as a basis for a short time to market and the economical implementation of hybrid solutions.