ST 010-13 Lohr am Main, 2013-09-06

More Power, Less Consumption: Mid-Range and Small Tractors Rely on Top-Range Functions

Dieter Fetting

Dieter Fetting, Director Sales and Industry Sector Management Agricultural and Forestry Machines at Bosch Rexroth AG

For almost a decade, growing affluence in emerging economies and the boom in renewable raw materials have fueled worldwide demand for agricultural and forestry machines. All indicators point to a continuation of this positive development. Two trends are shaping new machine concepts: Manufacturers are transferring functions previously reserved for the top-range segment to the mid- and low-range segments. This development mirrors the automotive industry: The anti-lock braking system (ABS) was first introduced on large sedan cars. Today it is fitted to almost every compact car. In parallel, pressure continues on manufacturers to maintain stringent exhaust emission limits and lower fuel consumption.

The Agritechnica 2013 shows that more and more tractor producers are fitting modern electro-hydraulic solutions previously reserved for the top-range segment to their mid- and low-range models. This applies, for instance, to double-acting electro-hydraulic hitch controls and load-sensing systems. They raise tilling efficiency, increase safety, and reduce fuel consumption and exhaust emissions. Tractor producers are systematically expanding their portfolios to include components and system solutions targeted at the volume market. Manufacturers are now integrating these efficient functions in smaller models.

Electro-hydraulic hitch control for simple tractors

Assemblies are now available for double-acting electro-hydraulic hitch control (EHC) on mid-range tractors. EHC improves tilling and reduces drive wheel slippage. This results in greater operator convenience and efficiency, while achieving lower fuel consumption at the same time. Studies show that suitably equipped tractors show up to 25% less slippage.

Bosch Rexroth has also developed a system solution for electro-hydraulic hitch control geared to the special requirements of emerging markets in the lower power range up to 80 HP, which is the best selling power segment worldwide. Starting 2014 a leading Indian manufacturer will equip serial production tractors with this system for the first time. This EHC variant is designed with extra ruggedness for vehicles without cab and to withstand high dust loads.

Demand-controlled power generation achieves significant benefits when it comes to fuel economy on smaller tractors fitted with higher levels of equipment. Now axial piston variable pumps are available for tractors of 50 HP and higher, permitting the implementation of load-sensing systems. New hydrostatic compact units for travel drives allow the use of modern power-split transmissions in the low HP range. The large number of new components and system solutions is accelerating technical progress in all tractor segments.

Further progress requires an overall system review

Vehicle manufacturers are networking mobile hydraulic systems with all other engine-related systems in order to harness the potential for lower fuel consumption, and therefore lower exhaust emissions. On their trade fair booth at Agritechnica, Bosch Rexroth is demonstrating the interdependence of these systems on a 1:1 functional model. It shows the large number of components affecting fuel consumption, from the engine, exhaust-gas after treatment, and mechanical transmissions for the travel drive, through to the various system and hybrid solutions for the hydraulics.

The individual modules influence each other mutually. Manufacturers can only achieve further progress in fuel economy and lower emissions by reviewing the system as a whole and the mutual dependence between each of the assemblies. To perform this complex task, they are resorting more and more frequently to the expertise of the Bosch Group, which is the only supplier to combine the technology fields of engine electronics, exhaust-gas after treatment, and mobile hydraulics under one roof.

At Bosch Rexroth, this expertise is systematically plowed in the development of new solutions and the optimization of existing solutions. As part of the Rexroth 4EE systematic (Rexroth for Energy Efficiency), this translates into Energy System Design – in other words, focusing on actual energy requirements – one of four key levers on which all development activities are based. Another three levers complete the 4EE system to assist manufacturers to optimize efficient energy use in their machines: Efficient Components describes raising efficiency and optimizing energy use with energy-efficient components. Energy Recovery refers to the storage of previously untapped energy for later use. Energy on Demand aims at optimizing demand control by switching off unrequired components to achieve the greatest possible energy savings.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, pneumatics, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 37,500 associates generated sales revenue of approximately 6.5 billion euros in 2012.

To learn more, please visit

The Bosch Group is a leading global supplier of technology and services, active in the fields of automotive technology, energy and building technology, industrial technology, and con-sumer goods. According to preliminary figures, more than 306,000 associates generated sales of 52.3 billion euros in 2012. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in some 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent some 4.5 billion euros for research and development in 2012, and applied for over 4,700 patents worldwide. The Bosch Group’s products and services are designed to fascinate, and to improve the quality of life by providing solutions which are both innovative and beneficial. In this way, the company offers technology worldwide that is “Invented for life.”

Additional information is available online at and


Search press releases


Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573