PI 101-13 Lohr am Main, 2013-09-17

Planetary Screw Assemblies: New Sizes Extend Application Spectrum in the Upper Range


Planetary screw assemblies from Rexroth offer high load capacities while featuring small installation dimensions for compact machine designs

Rexroth is going to offer screws having diameters of up to 75 mm and a lead of 20 mm

Rexroth opens up new fields of applications with planetary screw assemblies in new sizes. The drive elements with screw diameters up to 75 mm and leads up to 20 mm achieve static load capacities up to 1,496 kN while featuring a compact design. They are ideal for use in medium-sized and heavy-duty machinery such as presses, plastic injection molding machines and machine tools.

All electric presses and injection molding machines are reaching increasingly higher performance classes. This places more exacting demands on mechanical axis systems, which have to transmit increasingly greater forces. Rexroth now meets these requirements with planetary screw assemblies that feature diameters of 60 and 75 mm as well as leads of 10 and 20 mm each. Moreover, screw diameters of 20, 30, 39 and 48 mm with leads of 5 and 10 mm are available. The new sizes cover dynamic load capacities up to 544 kN and static load capacities up to 1,496 kN within a minimum of installation space. The drive units represent robust drive solutions for use in, for example, presses or plastic injection molding machines.

The design principle of planetary screw assemblies allows a high load capacity in relation to the installation dimensions. The planets rotate with a defined contact profile in a nut around a screw in parallel to the axis. This ensures very smooth running and reduces noise emission. Numerous contact faces result in high axial stiffness and load capacities, thus allowing for a long service life. These screw assemblies feature a high positioning accuracy and repeatability, also with minimal travel movements. In conjunction with a servo-motor and drive controller, the user gets a mechatronic unit from a single source, which moves large forces within a minimum of installation space.

Compact cylindrical single nuts, flange single nuts and split flange single nuts for all tolerance classes offer the designer a high degree of freedom. For applications with more demanding precision requirements, all nut types are available preloaded. This allows backlash-free movements in tolerance classes T7 and T5.

Rexroth’s innovative sealing technology in planetary screw assemblies results in long lubrication intervals. This reduces maintenance costs and spares the environment due to a lower consumption of lubricants.

In manufacturing the screws, Rexroth benefits from its experience in the efficient roll-forming process. This technology, which has proven successful in large series production, achieves the same accuracy levels as the more expensive grinding process. Rexroth supplies the planetary screw assemblies ready-to-install with machined ends.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, pneumatics, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 37,500 associates generated sales revenue of approximately 6.5 billion euros in 2012.

To learn more, please visit

The Bosch Group is a leading global supplier of technology and services. In fiscal 2012, its roughly 306,000 associates generated sales of 52.5 billion euros. Since the beginning of 2013, its operations have been divided into four business sectors: Automotive Technology, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 360 subsidiaries and regional companies in some 50 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent some 4.8 billion euros for research and development in 2012, and applied for nearly 4,800 patents worldwide. The Bosch Group’s products and services are designed to fascinate, and to improve the quality of life by providing solutions which are both innovative and beneficial. In this way, the company offers technology worldwide that is “Invented for life.”

Additional information is available online at and


Search press releases


Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573

Related Articles

Press Information

The five most expensive savings ideas for the maintenance of machinery and equipment

Machine downtime is always expensive, especially if a whole production line comes to a standstill as a result. For new machinery, the machine manufacturer is still liable, but afterwards the responsibility for maintenance lies solely with the user. Maintenance staff must constantly justify their "unproductive" costs and, hence, try to reduce them. However, some short-term saving ideas lead to nothing but higher total costs in the end. The following are the five most expensive, and unfortunately, not uncommon errors when it comes to machine maintenance.


The factory of the future creates added value through flexibility and agility

In future production environments demands on adaptability will rise. This development can only be realized by separating hardware and software in automation. Bosch Rexroth AG promotes this development primarily with a broad product spectrum from sensors to drive and control technology to software solutions.