PI 099-13n 2013-09-25

Pumps at a record height

Nowhere else do cities grow faster than in China these days. In order to keep up with this growth, the house builders need respective construction equipment and here, engineering ingenuity of Bosch Rexroth comes into play. The new mobile concrete pump of the Chinese machinery manufacturer Zoomlion is an impressive example. With exactly 101.18 meters, it impressively rises into the sky ‒ this even caught the attention of the Guinness Book of Records. Apart from the pure size, Zoomlion also convinces with its technology: a glimpse into the inside of the concrete pump, discloses hydraulics from Rexroth. The main component is the piston pump A4VG. It provides everything that the fast construction industry in China requires: high operating pressure, high displacement volume and many sensible highly integrated functions.

Copyright image: Bosch Rexroth AG


Search press releases


Ingrid Alter
Löwentorstraße 68-70
70376 Stuttgart
Phone: +49 711 811-30849