International
 

Press

Content
PI 104-13 Lohr am Main, 2013-10-04

Completely Modular and Ultra-Efficient

Modular and configurable down to the last detail: MSC mini slides

The new generation of MSC mini slides from Rexroth Pneumatics can be configured to perfectly fit your requirements.

The MSC series mini slides have a compact design, require minimal installation space and can be optimally configured for virtually any automated handling task. The new generation of mini slides offers a multitude of variants and equipment details.

Its numerous configuration options make the mini slide a truly universal handling component. Diameter, stroke length, performance of the guiding, number of pistons, and air connections are all easy to define with the intuitive configurator, which can also be used to select the type of cushioning, end position lock, or accessories. Custom-configured for specific applications, the mini slides are an efficient component for any handling task.

With the special Easy-2-Combine interface, the mini slides can be combined with other components in a handling system as required, without the need for additional mounting plates. Its direct connection to rotary modules, rodless cylinders, and further slide units or grippers makes the MSC series ideal for various tasks in many different industries, especially in the areas of automation and handling.

The MSC's small cross-section allows for especially compact machine designs. Depending on the installation situation, sensors, stroke setting, and air connections can be installed on both sides. The symmetrical design also enables parallel mounting of two mini slides. The pre-tensioned guide system without play and one-piece slide table offers maximum stability and reliable precision with minimal tolerance values – even for high torque absorption and load capacities.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, pneumatics, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 37,500 associates generated sales revenue of approximately 6.5 billion euros in 2012.

To learn more, please visit www.boschrexroth.com

The Bosch Group is a leading global supplier of technology and services. In fiscal 2012, its roughly 306,000 associates generated sales of 52.5 billion euros. Since the beginning of 2013, its operations have been divided into four business sectors: Automotive Technology, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 360 subsidiaries and regional companies in some 50 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent some 4.8 billion euros for research and development in 2012, and applied for nearly 4,800 patents worldwide. The Bosch Group’s products and services are designed to fascinate, and to improve the quality of life by providing solutions which are both innovative and beneficial. In this way, the company offers technology worldwide that is “Invented for life.”

Additional information is available online at www.bosch.com and www.bosch-press.com

 

Search press releases


Contact

Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573
susanne.herzlieb@boschrexroth.de




Related Articles

2013-09-16
Corporate Information

Triton to acquire Bosch Rexroth pneumatics business

Bosch Rexroth plans to sell its global pneumatics business (Rexroth Pneumatics) to the German-Scandinavian investor Triton. Agreements to this effect were signed. It has been agreed that the purchase price will not be disclosed. The acquisition is subject to approval by the antitrust authorities.