PI 116-13 Lohr am Main, 2013-11-20

Easy to implement gesture control in automation

With the new generation of Rexroth control units, machinery manufacturers apply a familiar gesture control from smart devices to the field of automation.

Configuring the new Rexroth IndraControl V control units with a uniform software tool

With the swipe of a finger through the program: With a new generation of control units, Bosch Rexroth now brings the advantages of gesture control, which is familiar from smartphones and tablet PCs, to automation. The robust family of devices is designed for use in harsh production conditions and is available in different display sizes. A single software tool simplifies the implementation.

To scroll, just swipe the screen or use two fingers to zoom in on a part of the image: the gesture control has become prevalent in private applications through smartphones and tablet PCs within just a few years.

With a new generation of multi-touch control units from Rexroth, machine manufacturer can also use this operating philosophy in factory automation. In the process, Bosch Rexroth simplifies the configuration of user interfaces through a single software tool for all HMI devices. WinStudio enables efficient engineering through the reuse of software modules – across the entire spectrum of controller-based compact HMIs with Windows CE to large displays for industrial PCs.

Thus, the new compact miniature control units, with a 4 to 9 inch diagonal display and their own controller, are offered for both single- and multi-touch operation. The communication with a control unit occurs, according to standard, over a fast Ethernet TCP IP connection. For purposes of data backup, the devices have an SD card memory module and 2 USB ports for connecting peripheral devices.

New wide-screen displays for 15, 18 and 21 inch industrial PCs provide plenty of space for a high depth of information and a modern multi-touch visualization of PC-based automation applications. The aluminum front with inlaid, scratch-resistant glass meets protection category IP65. Together with the high shock and vibration resistance, the operating units are therefore suitable for use under rough production conditions.

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, pneumatics, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 37,500 associates generated sales revenue of approximately 6.5 billion euros in 2012.

To learn more, please visit

The Bosch Group is a leading global supplier of technology and services, active in the fields of automotive technology, energy and building technology, industrial technology, and consumer goods. According to preliminary figures, more than 306,000 associates generated sales of 52.3 billion euros in 2012. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in some 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent some 4.5 billion euros for research and development in 2012, and applied for over 4,700 patents worldwide. The Bosch Group’s products and services are designed to fascinate, and to improve the quality of life by providing solutions which are both innovative and beneficial. In this way, the company offers technology worldwide that is “Invented for life”.

Additional information is available online at and


Search press releases


Susanne Herzlieb
Maria-Theresien-Straße 23
97816 Lohr am Main
Phone: +49 9352 18-1573

Related Articles

Press Information

Flexible, continuous production

The growth markets of energy storage and printed electronics are characterized by considerable pressure in terms of time, quality and costs. Bosch Rexroth positions itself as an incredibly reliable automation partner, delivering easy-to-integrate system solutions to handle the current challenges in the printing, semiconductor and display industry. For example, the flexible transport system FTS suitable for vacuum applications and the precision motion control MPC accurate to the nanometer demonstrate how roll-to-roll, coating and production processes can be continuously optimized and made future proof.

Product Information

Software drives innovation

Vertical and horizontal connectivity, digital engineering, economic production of very small batch sizes – without software, these core characteristics of Industry 4.0 would be inconceivable. Even today, software contributes a great deal to the added value created by machines, while in the factory of the future it supplies the necessary intelligence for modular, mobile and connected production components. Using its Connected Automation portfolio, Bosch Rexroth will be demonstrating how state-of-the-art software affects competitiveness and time-to-market at the SPS IPC Drives.