Marginal Column

Prevention made simple

Content

July 2017

 

Predictive maintenance reduces system downtimes and thus saves time and money.

Unexpected machine downtimes are a nightmare for every production manager. Particularly in large plants that produce around the clock, such as mines, foundries, or rubber compound plants, every hour a machine is not running is linked to extremely high costs. Forward-looking maintenance is a reliable method of reducing expensive plant downtimes in practice.

The ODiN (Online Diagnostics Network) service package from Bosch Rexroth uses the interaction of sensors, cloud-based applications, and machine learning methods to monitor operating conditions based on models and to carry out predictive maintenance activities. During the teach-in period, a machine learning algorithm identifies a normal healthy condition from a variety of sensor signals, for example pressure, flow, vibration, temperature, and oil quality, according to the assembly to be monitored.

After the teach-in phase, ODiN uses the data-based model to continuously calculate a health index for the monitored assembly. If a single measured value moves outside the tolerance range for a short time, this does not necessarily lead to a (false) warning, as wear can rarely be detected with just one signal. If the health index deteriorates due to changes in the data from multiple sensors within the defined limits because the behavior of the machine has changed, the system warns of a problem. The health index generated not only indicates the status of the actual assembly being monitored, but also more gradual changes in the upstream and downstream mechanical or hydraulic systems. If movements start to take longer or require more power over time, this is a sign of wear in the mechanical or hydraulic system.

An example data record shows how much of a complex task wear diagnosis can be: From a statistical perspective, the probability of a fault being randomly discovered is just 13 percent. An expert who uses traditional methods to continuously monitor the system will have a 43 percent probability of detecting it. However, the system has a fault detection rate of over 95 percent. The software can either precisely identify the fault, or it supports maintenance engineers with troubleshooting by localizing the fault to a particular assembly.

Prevention made simple

Prevention made simple