Products
OverviewIndustries
OverviewService
OverviewBuy
OverviewCompany
OverviewProduct groups
OverviewEngineering
OvervieweConfigurators and Tools
OverviewEDI (Electronic Data Interchange)
OverviewAgDrive, an efficient complete solution from Bosch Rexroth which includes BODAS Software, opens up a wide range of functions for self-propelled agricultural machines with a hydrostatic multi-motor drive
With the hydrostatic AgDrive travel drive solution for self-propelled agricultural machines, Bosch Rexroth presents a new complete package comprising software and drive components. It enables manufacturers of off-highway vehicles to build travel drives in accordance with the ISO 25119 standard in a particularly economical manner. Manufacturers can choose from two software versions: The easily parameterizable ASrun software or the individually adaptable and expandable ASopen software from the BODAS modular system. The software which is available in the Try it First program can be downloaded and used on a trial basis free of charge. The functional highlights of the travel drive solution include Fulldrive Control and Dynamic Traction Force Distribution.
The demands as regards self-propelled agricultural machines with hydrostatic multi-motor drives are growing all the time. In order to ensure the necessary performance and productivity, the market expects an ever wider range of functions. In the case of machines with a number of hydraulic motors, this automatically results in a complex design. This applies in particular to software development which has to meet exacting safety requirements at the same time.
The complete AgDrive solution enables machine manufacturers to implement future-proof travel drives without lengthy and costly development work on the basis of high-end drive components and multifunctional software modules which are easy to apply and expand. The most important new features include Fulldrive Control – a cruise control system with braking function – and Dynamic Traction Force Distribution. AgDrive also offers advanced functions such as High Level Braking (HLB), drive-slip control (ASR) and an electro-hydraulic anti-lock braking system (ABS).
Thanks to “Try it First”, manufacturers can download the BODAS AgDrive software in advance, add extra functions, adapt it to their own needs, test it and ultimately only adopt what they actually use.
Less application work in spite of complex functions with cutting-edge features
The BODAS AgDrive software with Rexroth’s new BODAS RC/40 control units significantly reduces the application work for machine manufacturers looking to individually customize their systems. As a result, complex functions for mobile machines can be implemented easily and flexibly. The ASrun software version enables customers to parameterize the travel drive functions according to their specific requirements without development work and with little effort. The ASopen version also allows existing functions for individually controlling the travel drive components to be expanded.
The BODAS AgDrive software was developed taking into account the ISO 25119 safety standard, so that if the safety functions are suitable for the intended use, no additional development work is required to meet the safety-related specifications. This means that the mobile machine can be used immediately once the software has been parameterized. If necessary, the software can also be configured to meet the requirements of ISO 13849 and ISO 19014.
Bosch Rexroth at Agritechnica: Hall 16, Booth A08.
Media Assets
Basic Information Bosch Rexroth
As one of the world’s leading suppliers of drive and control technologies, Bosch Rexroth ensures efficient, powerful and safe movement in machines and systems of any size. The company bundles global application experience in the market segments of Mobile and Industrial Applications as well as Factory Automation. With its intelligent components, customized system solutions, engineering and services, Bosch Rexroth is creating the necessary environment for fully connected applications. Bosch Rexroth offers its customers hydraulics, electric drive and control technology, gear technology and linear motion and assembly technology, including software and interfaces to the Internet of Things. With locations in over 80 countries more than 32,000 associates generated sales revenue of around 7.0 billion euros in 2022.
Basic Information Bosch
The Bosch Group is a leading global supplier of technology and services. It employs roughly 421,000 associates worldwide (as of December 31, 2022). The company generated sales of 88.2 billion euros in 2022. Its operations are divided into four business sectors: Mobility, Industrial Technology, Consumer Goods, and Energy and Building Technology. As a leading IoT provider, Bosch offers innovative solutions for smart homes, Industry 4.0, and connected mobility. Bosch is pursuing a vision of mobility that is sustainable, safe, and exciting. It uses its expertise in sensor technology, software, and services, as well as its own IoT cloud, to offer its customers connected, cross-domain solutions from a single source. The Bosch Group’s strategic objective is to facilitate connected living with products and solutions that either contain artificial intelligence (AI) or have been developed or manufactured with its help. Bosch improves quality of life worldwide with products and services that are innovative and spark enthusiasm. In short, Bosch creates technology that is “Invented for life.” The Bosch Group comprises Robert Bosch GmbH and its roughly 470 subsidiary and regional companies in over 60 countries. Including sales and service partners, Bosch’s global manufacturing, engineering, and sales network covers nearly every country in the world. The basis for the company’s future growth is its innovative strength. At 136 locations across the globe, Bosch employs some 85,500 associates in research and development, of which nearly 44,000 are software engineers.
Press Contact
Spokesperson technology topics
Manuela Kessler
+49 9352 18-4145
Manuela.Kessler@boschrexroth.de