1. Home
  2. Company
  3. Press Portal
transfer system TS 7plus
transfer system TS 7plus
Press release

Standardized construction kit for heavy-duty transport: roller conveyor TS 7plus transports up to 3,000 kg through assembly lines

  • World’s first freely configurable, fully-electric transfer system for heavy loads
  • Highly available standard components replace individual projects
  • Segmented operation increases energy efficiency

Battery packs for e-mobility, e-axles, and other heavy components demand new concepts for material flow in assembly. Commonly used, customized individual projects are very complex, while automated guided vehicles (AGVs) often increase transport times. Bosch Rexroth is closing this gap with the new roller conveyor TS 7plus. Based on a standardized construction kit, the heavy-duty transfer system efficiently transports workpieces weighing up to 3,000 kg through assembly lines.

The transfer systems TS 1, TS 2plus, and TS 5 from Bosch Rexroth are widely used in the automotive industry across the world. They move small and medium-sized workpieces through assembly lines in a highly efficient manner. The transfer system TS 7plus is the world’s first solution to apply this modular approach to workpieces weighing up to 3,000 kg. The standard dimensions of the workpiece pallets are up to 2,200 x 3,000 mm.

TS 7plus transports material via conveyor rollers on freely configurable modular sections with lift/transverse, rotary, and positioning units, as well as stop gates. The 350mm minimum possible transportation height for both longitudinal and transverse conveying helps facilitate manual processes and improves ergonomics for employees.

The conveyor section consists of either solid or hollow rollers, which are approximately 50 percent larger than the previous TS 7 system. The reduced number of moving parts per meter increases availability and the newly designed bearing block enables faster assembly with two screw points in the profile, as well as easy replacement for maintenance.

Lubrication-free king shaft

Unlike chain drives, the tried-and-tested drive via king shafts operates without lubrication and requires minimal maintenance. The motor’s torque is transmitted to the conveyor rollers via bevel wheels, thus minimizing contamination of the workpieces. The bevel wheels also require no re-tensioning or maintenance.

In conventional accumulation operation, stop gates keep the workpiece pallets at defined stations. With the alternative segmented operation, the motors for section transport, rotary units, and lift/transverse units run only when required. This increases energy efficiency across the entire life cycle and significantly reduces the total cost of ownership. In addition, the motors can be designed smaller and benefit from a longer service life due to their demand-based operation. As part of its system portfolio, Bosch Rexroth offers motors with outputs of 180 W and 250 W for the TS 7plus, as well as an interface for the use of third-party motors.

High conveyor speed, no interfering contours

The motors can be placed on either the outside or inside of the section. With internally mounted motors, there are no interfering contours that could otherwise hinder employees or protrude into travel paths. With a conveyor speed of up to 24 m/min, the system achieves significantly shorter transport times than automated guided vehicles (AGVs), for example.

CAD-free configuration with planning software MTpro

The intuitive planning software MTpro assists in the configuration of transfer systems, and guides users quickly and easily through the whole process. Bosch Rexroth offers the planning software as a locally installable full version and as an installation-free web version in the form of MTpro online Designer. The software automatically creates CAD models and parts lists from builds, which can be transferred to the Rexroth Store or to certified partners.

Media Assets

Here you can download the images from this Press Release

Basic Information Bosch Rexroth

As one of the world’s leading suppliers of drive and control technologies, Bosch Rexroth ensures efficient, powerful and safe movement in machines and systems of any size. The company bundles global application experience in the market segments of Mobile and Industrial Applications as well as Factory Automation. With its intelligent components, customized system solutions, engineering and services, Bosch Rexroth is creating the necessary environment for fully connected applications. Bosch Rexroth offers its customers hydraulics, electric drive and control technology, gear technology and linear motion and assembly technology, including software and interfaces to the Internet of Things. With locations in over 80 countries, around 32,600 associates generated sales revenue of 6.5 billion euros in 2024.

Basic Information Bosch

The Bosch Group is a leading global supplier of technology and services. It employs roughly 413,000 associates worldwide (as of December 31, 2025). The company generated sales of 91 billion euros in 2025. Its operations are divided into four business sectors: Mobility, Industrial Technology, Consumer Goods, and Energy and Building Technology. With its business activities, the company aims to use technology to help shape universal trends such as automation, digitalization, electrification, and artificial intelligence. In this context, Bosch’s broad diversification across regions and industries strengthens its innovativeness and robustness. Bosch uses its proven expertise in hardware, software, and services to offer customers cross-domain solutions from a single source. It also applies its expertise in connectivity and artificial intelligence in order to develop and manufacture intelligent, user-friendly, and sustainable products. With technology that is “Invented for life,” Bosch wants to help improve quality of life and conserve natural resources. The Bosch Group comprises Robert Bosch GmbH and its roughly 500 subsidiary and regional companies in over 60 countries. Including sales and service partners, Bosch’s global manufacturing, engineering, and sales network covers nearly every country in the world. Bosch’s innovative strength is key to the company’s further development. Bosch employs some 82,000 associates in research and development.

Press Contact

Please get in touch with our Press Contact
Manuela Kessler - spokesperson technology topics

Spokesperson technology topics
Manuela Kessler
+49 9352 18-4145
Manuela.Kessler@boschrexroth.de

Related News

Assembly Technology

23/06/2025

Maximum freedom and process reliability

The new cordless nutrunner NEXO from Bosch Rexroth provides production companies with intuitive, modern and user-friendly tools with significantly improved ergonomics and reliable performance.

Read More
Assembly Technology
Industrial Hydraulics
Linear Motion Technology
Electric Drives and Controls

31/03/2025

Hannover Messe 2025

Bosch Rexroth presents future-proof hydraulics, open automation solutions and AI-based services at Hannover Messe.

Read More
Assembly Technology
Linear Motion Technology
Assembly and Handling
Automation and Electrification Solutions
Automation for Battery Production

12/03/2025

Battery production in the gigafactory: Bosch Rexroth presents solution portfolio at the Battery Show Europe

With a combination of real exhibits and a virtual gigafactory, Bosch Rexroth is showcasing selected process steps of high-performance battery production at the Battery Show Europe.

Read More