Compact, heavy-duty axis with two carriages optimizes space requirements and cycle times of dynamic handling applications
Bosch Rexroth is expanding its CKR series of compact modules with an innovative dual belt axis for dynamic handling with a total load capacity of up to 770 kg. The new CKR-280 heavy-duty axis combines the functions of two linear axes into one linear system. Two, independently driven carriages in a single frame enable dynamic applications with high drive torques and short cycle times. The compact, dual-handling system reduces valuable installation space and increases productivity, while saving time and costs for engineering, assembly and commissioning. The new solution can be utilized as a single axis or combined with other linear axes into a multi-axis system, with the option also to include a drive package.
Whether in battery production, intralogistics or machine tool automation, many industries are increasingly seeking compact handling solutions that can move large payloads with high dynamics. With the new dual belt version of the CKR compact module series in size 280, Bosch Rexroth offers a space-optimized, heavy-duty axis that can handle two payloads up to 385 kg each and drive torques up to 250 Nm.
To enable fast and easy engineering, the compact modules can be configured online in lengths up to 5.50 m. Bosch Rexroth can also deliver longer travel ranges on request. High accelerations of up to 5g and a maximum speed of 5 m/s provide the optimal conditions for short cycle times with high precision and a repeatability of +/- 0.05 mm. Depending on the requirements, a variety of travel profiles can be implemented independently.
After its market launch, the CKR-280 heavy-duty axis will also be integrated into the e-tool chain as a new size for single-axis and multi-axis systems.
For more information on Bosch Rexroth’s complete line of compact module solutions, please visit boschrexroth-us.com.
Media Assets
Basic Information Bosch Rexroth
As one of the world’s leading suppliers of drive and control technologies, Bosch Rexroth ensures efficient, powerful and safe movement in machines and systems of any size. The company bundles global application experience in the market segments of Mobile and Industrial Applications as well as Factory Automation. With its intelligent components, customized system solutions, engineering and services, Bosch Rexroth is creating the necessary environment for fully connected applications. Bosch Rexroth offers its customers hydraulics, electric drive and control technology, gear technology and linear motion and assembly technology, including software and interfaces to the Internet of Things. With locations in over 80 countries, around 32,600 associates generated sales revenue of 6.5 billion euros in 2024.
Basic Information Bosch
The Bosch Group is a leading global supplier of technology and services. It employs roughly 417,900 associates worldwide (as of December 31, 2024). According to preliminary figures, the company generated sales of 90.5 billion euros in 2024. Its operations are divided into four business sectors: Mobility, Industrial Technology, Consumer Goods, and Energy and Building Technology. With its business activities, the company aims to use technology to help shape universal trends such as automation, electrification, digitalization, connectivity, and an orientation to sustainability. In this context, Bosch’s broad diversification across regions and industries strengthens its innovativeness and robustness. Bosch uses its proven expertise in sensor technology, software, and services to offer customers cross-domain solutions from a single source. It also applies its expertise in connectivity and artificial intelligence in order to develop and manufacture user-friendly, sustainable products. With technology that is “Invented for life,” Bosch wants to help improve quality of life and conserve natural resources. The Bosch Group comprises Robert Bosch GmbH and its roughly 470 subsidiary and regional companies in over 60 countries. Including sales and service partners, Bosch’s global manufacturing, engineering, and sales network covers nearly every country in the world. Bosch’s innovative strength is key to the company’s further development. At 136 locations across the globe, Bosch employs some 86,900 associates in research and development, of which nearly 48,000 are software engineers.
Press Contact
Lauren Partenheimer
+1 847-645-3636
Lauren.Heinz@boschrexroth-us.com